Hi everyone,
I'm currently progress in booting Linux (Arago distribution from the PSP) on a custom board made by my company based on an OMAP L138.
The board is populated with two microSD slots. Signals are respectively connected to MMCSD0 and MMCSD1 pins on the OMAP L138. I made some changes to the "board-da850-evm.c" file so that the module provided by Ti for Linux can "recognize" the memory card into the first slot. Linux is now able to read and/or write files to the memory card on the first slot.
Unfortunately, Linux do not "recognize" the memory card on the second slot. Can someone tell me the procedure?
Thanks in advance!
Best regards,
Térence