Part Number: AM625
Hi Team,
We have started working on the MCAN module configuration for the AM625 Development Board.
Modified the below parameters in the device tree file.
1. Enabled the MCAN0 instance in the main domain (main_mcan0).
=> To enable the can0 interface
2. GPIO Pins used:
C15 --> MCAN0_TX_GPIO1_24, Base Address 0x01d8
E15 --> MCAN0_RX_GPIO1_25, Base Address 0x01dc
3. We are trying to check for the loopback functionality of MCAN
Please suggest the changes required to enable the MCAN feature on AM625 development board.
Thanks.