This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: Help Configure Pins

Part Number: SK-AM62B-P1


I don't understand the hex numbers used on the pin configuration:

main_mmc2_pins_default: main-mmc2-pins-default {
		pinctrl-single,pins = <
			AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */
			AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */
			AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */
			AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */
			AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */
			AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */
			AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */
		>;
	};

I'm trying to use pin "IO_EXP_TEST_LED" on the "TCA64WRARGJR" IO Expander, but don't know what configuration I need.

I find on "k3-am625-sk.dts" this:

&main_i2c1 {
	exp1: gpio@22 {
		compatible = "ti,tca6424";
		reg = <0x22>;
		gpio-controller;
		#gpio-cells = <2>;
		gpio-line-names = "GPIO_CPSW2_RST", "GPIO_CPSW1_RST",
				   "PRU_DETECT", "MMC1_SD_EN",
				   "VPP_LDO_EN", "EXP_PS_3V3_En",
				   "EXP_PS_5V0_En", "EXP_HAT_DETECT",
				   "GPIO_AUD_RSTn", "GPIO_eMMC_RSTn",
				   "UART1_FET_BUF_EN", "WL_LT_EN",
				   "GPIO_HDMI_RSTn", "CSI_GPIO1",
				   "CSI_GPIO2", "PRU_3V3_EN",
				   "HDMI_INTn", "PD_I2C_IRQ",
				   "MCASP1_FET_EN", "MCASP1_BUF_BT_EN",
				   "MCASP1_FET_SEL", "UART1_FET_SEL",
				   "TSINT#", "IO_EXP_TEST_LED";

		interrupt-parent = <&main_gpio1>;
		interrupts = <23 IRQ_TYPE_EDGE_FALLING>;
		interrupt-controller;
		#interrupt-cells = <2>;

		pinctrl-names = "default";
		pinctrl-0 = <&main_gpio1_ioexp_intr_pins_default>;
	};
};

and then later I see that the phandle "exp1" is being used like this:

wlan_lten: regulator-6 {
		compatible = "regulator-fixed";
		regulator-name = "wlan_lten";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		vin-supply = <&vcc_3v3_sys>;
		gpios = <&exp1 11 GPIO_ACTIVE_LOW>;
	};

So I imagine I would have to do something similar?

  • Hi Alexandre,

    I don't understand the hex numbers used on the pin configuration:

    The hex numbers are offset of the pin PADCONFIG register.

    So I imagine I would have to do something similar?

    Yes or No, depending on how exactly you want to use this IO_EXP_TEST_LED pin, from Linux user space or kernel space. This "&exp1 11" example is only for the usage in kernel, it is not needed when you want to control the exp1 GPIO in Linux user space.