This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: Need help to toggle the GPIO1_49 pins on AM62X EVK

Part Number: PROCESSOR-SDK-AM62X

Hi,

Actually i have assigned work to on/off toggle the GPIO1_49 pin on AM62X EVK. When we type the command :- echo default-on > sys/class/leds/am62-sk\:green\:heartbeat/trigger then this  gpio continually remain on.

But i need it ON/OFF through terminals like echo out > direction ; cat value ;- 0 or echo in > direction; cat value:- 1 . Is it possible to do it ? 

Please explain step by step if it is .

Regards,

Dnyaneshwar