Other Parts Discussed in Thread: TVP5158
SDK the latest one;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TVP5158
SDK the latest one;
DM8168 can have more than 4 channels input. For example if board supports video encoder chip TVP5158, it can capture 16 D1 signals.
For creating more than 4 channels of decode, may be you are running short of memory allocated by default. You can see the media controller logs
by doing /usr/share/ti/ti-uia/loggerSMDump.out 0x9e400000 video.
For changing memory following link can be used;
Thanks Vimal,
I change the meory map( MC_HDVICP2_INT_HEAP_CACHED & IPC_SR_FRAME_BUFFERS ) by http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map
,Then, Can decode 4 HD channels & run without any err,but when i create the fifth decoder,it can create,but, setting the decoder to idle state and alloc the input & output buffers,it failed.( No matter how much memory I allocated )
Use system_top Command output:
sys_top Ver : 0.2.0.0
Number Of Running Cores: 3
DSP :
Not Running or Do not integrate sys_top functionality
MC.HDVICP2:
0 Heap:Size 1048576 Used 567048 MaxU 567048 Free 481528 LarF 481192
Num SR :4
SRIn 0 :PhyA 0x9f700000 Virt 0x0 Size 0x200000
SRHeap:Size 2095488 Used 19840 MaxU 19840 Free 2075648 LarF 2075648
SRIn 1 :PhyA 0x9a100000 Virt 0x0 Size 0x100000
SRHeap:Size 1048448 Used 0 MaxU 0 Free 1048448 LarF 1048448
SRIn 2 :PhyA 0x9f900000 Virt 0x0 Size 0x10000000
SRHeap:Size 268435328 Used 8559360 MaxU 8559360 Free 259875968 LarF 259875968
MC.HDVPSS:
0 Heap:Size 2097152 Used 107568 MaxU 107568 Free 1989584 LarF 1989584
1 Heap:Size 28311552 Used 0 MaxU 0 Free 28311552 LarF 28311552
Num SR :4
SRIn 0 :PhyA 0x9f700000 Virt 0x0 Size 0x200000
SRHeap:Size 2095488 Used 19840 MaxU 19840 Free 2075648 LarF 2075648
SRIn 1 :PhyA 0x9a100000 Virt 0x0 Size 0x100000
SRHeap:Size 1048448 Used 0 MaxU 0 Free 1048448 LarF 1048448
SRIn 2 :PhyA 0x9f900000 Virt 0x0 Size 0x10000000
SRHeap:Size 268435328 Used 8559360 MaxU 8559360 Free 259875968 LarF 259875968
/usr/share/ti/ti-uia/loggerSMDump.out 0x9e400000 video output:
N:Video P:1 #:00831 T:00000024|9bd07869 S:Entered: OMX_BASE_DIO_Init (0x9da21d10, 1, OMX.DIO.NONTUNNEL, 0x9da2168c)
N:Video P:1 #:00832 T:00000024|9bd11ab5 S:Module<OMX.TI.DUCATI.VIDDEC> Leaving<OMX_BASE_DIO_Init> @line<172> with error<0:ErrorNone>
N:Video P:1 #:00833 T:00000024|9bd17b25 S:Module<OMX.TI.DUCATI.VIDDEC> Entering<OMX_BASE_DIO_Open> @line<252>
N:Video P:1 #:00834 T:00000024|9be04f5f S:Module<OMX.TI.DUCATI.VIDDEC> Leaving<OMX_BASE_DIO_Open> @line<257> with error<0:ErrorNone>
N:Video P:1 #:00835 T:00000024|9be1bbbd S:OMX_TI_VIDDEC_CommandNotify::Line 2118::VDEC Error->VIDDEC3_create Failed
N:Video P:1 #:00836 T:00000024|9be2ee77 S:Entered Function :omxrpc_skel_allocbuffer
N:Video P:1 #:00837 T:00000024|9be6318b S:Entered Function :omxrpc_skel_allocbuffer
N:Video P:1 #:00838 T:00000024|9be94dd9 S:Entered Function :omxrpc_skel_allocbuffer
N:Video P:1 #:00839 T:00000024|9bec7119 S:Entered Function :omxrpc_skel_allocbuffer
N:Video P:1 #:00840 T:00000024|9bf08669 S:Module<OMX.TI.DUCATI.VIDDEC> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<786> with error<-2147479552:ErrorInsufficientResources>
N:Video P:1 #:00841 T:00000024|9bf10d3d S:Module<OMX.TI.DUCATI.VIDDEC> Leaving<OMX_BASE_CmdEventHandler> @line<468> with error<-2147479552:ErrorInsufficientResources>
N:Video P:1 #:00842 T:00000024|9bf1896f S:Module<OMX.TI.DUCATI.VIDDEC> Entering<OMX_BASE_CmdEventHandler> @line<437>
N:Video P:1 #:00843 T:00000024|9bf1e5ff S:Module<OMX.TI.DUCATI.VIDDEC> Leaving<OMX_BASE_CmdEventHandler> @line<468> with error<0:ErrorNone>
Setting error?Can anyone tell me how to set it? Thanx;
Are you trying HD channels or smaller resololution. Could you please try say CIF or QCIF resolution to test if you can create > 4 channels. Most likely it should be heap running out of memory.
Regards
Vimal
According to your reply, I tried create 5 CIF (also QCIF)channels to test ,There is still the same problem. Can't set decoders to idle state.
But the same Program, running under ezsdk5_01_01_80,can create 5 CIF channels and runing without any err,but this SDKjust allow me to create only one HD channel(>1 will failed).
Are there examples that Successfully decoding multiple-channlel video ?
Thanks
As per your earlier post "Can decode 4 HD channels & run without any err"
so It confuses now, when you say > 1 will fail. We have tried 2 HD decoder, and some community members have also tried 2 HD decode and that works. we will check for >4 D1 decoders.
Regards
Vimal
I'm sorry for my bad expression. It can decoding 4 HD channels(also 4 D1 channels,but more will fail) by using ezsdk5_02_01_59,
can decoding 1 HD channel( 5 D1 channels) by using ezsdk5_01_01_80.
Thanx