Other Parts Discussed in Thread: TDA4VH
Hi TI Experts,
Customer is working on TDA4VH SDK9.1.
They are doing the TOG module initialization on MCU1-1.
However, when they use ESM callback function they found the below error.
The callback function is below.
They also read the ESM register below.
The error information got from the register is below.
Could you help provide some suggestions about what could cause these problems please?
Another question is that, customer does not know the meaning of the STOG index below. We cannot find this information on TRM.
Actually the reason why customer did the TOG module initialization is to follow the SDL_SA_0006 requirement in the SDL Safety Manual. They do not know if they have to initialize all of the above STOG instances, or just a part of them is enough.
Please help provide some suggestions on this please, thanks for that!
Kind Regards,
Kevin