This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM68: DisplayPort resolution defaults to 800x600 when monitor is capable of 1920x1080.

Part Number: SK-AM68
Other Parts Discussed in Thread: TDA4VM,

I'm running SDK version 09_01_00 on my SK-AM68A dev board.  It powers up with an 800x600 resolution on my monitor.  My monitor is capable of 1920x1080, so that's what I'm expecting to see.

If I connect the same monitor to a TDA4VM dev kit also running SDK version 09_01_00, the output resolution is 1920x1080 which is what I expect.

How do I get my SK-AM68 to output a higher resolution?  Is this a function of a device tree overlay or something else?

  • I mention it in the title but not in the post above: I'm connected via the DisplayPort interface.

    Here's what I see when I run `weston-info`.  It only is displaying a single video mode when I expect several:

    *** Please use wayland-info instead
    *** weston-info is deprecated and will be removed in a future version

    interface: 'wl_compositor', version: 4, name: 1
    interface: 'wl_subcompositor', version: 1, name: 2
    interface: 'wp_viewporter', version: 1, name: 3
    interface: 'zxdg_output_manager_v1', version: 2, name: 4
    xdg_output_v1
    output: 18
    name: 'eDP-1'
    logical_x: 0, logical_y: 0
    logical_width: 800, logical_height: 600
    interface: 'wp_presentation', version: 1, name: 5
    presentation clock id: 1 (CLOCK_MONOTONIC)
    interface: 'zwp_relative_pointer_manager_v1', version: 1, name: 6
    interface: 'zwp_pointer_constraints_v1', version: 1, name: 7
    interface: 'zwp_input_timestamps_manager_v1', version: 1, name: 8
    interface: 'wl_data_device_manager', version: 3, name: 9
    interface: 'wl_shm', version: 1, name: 10
    formats: 'XB30'(0x30334258) 'AB30'(0x30334241) 'XYUV'(0x56555958) 'YUYV'(0x56595559) 'NV12'(0x3231564e) 'YU12'(0x32315559) RGB565 XRGB8888 ARGB8888
    interface: 'weston_touch_calibration', version: 1, name: 11
    interface: 'wl_drm', version: 2, name: 12
    interface: 'wl_seat', version: 7, name: 13
    name: default
    capabilities: keyboard
    keyboard repeat rate: 40
    keyboard repeat delay: 400
    interface: 'zwp_linux_dmabuf_v1', version: 4, name: 14
    formats:
    'YV12'(0x32315659), modifier: 0x0000000000000000
    'YV12'(0x32315659), modifier: 0x00ffffffffffffff
    'YU12'(0x32315559), modifier: 0x0000000000000000
    'YU12'(0x32315559), modifier: 0x00ffffffffffffff
    'NV21'(0x3132564e), modifier: 0x0000000000000000
    'NV21'(0x3132564e), modifier: 0x00ffffffffffffff
    'NV12'(0x3231564e), modifier: 0x0000000000000000
    'NV12'(0x3231564e), modifier: 0x00ffffffffffffff
    'YVYU'(0x55595659), modifier: 0x0000000000000000
    'YVYU'(0x55595659), modifier: 0x00ffffffffffffff
    'VYUY'(0x59555956), modifier: 0x0000000000000000
    'VYUY'(0x59555956), modifier: 0x00ffffffffffffff
    'UYVY'(0x59565955), modifier: 0x0000000000000000
    'UYVY'(0x59565955), modifier: 0x00ffffffffffffff
    'YUYV'(0x56595559), modifier: 0x0000000000000000
    'YUYV'(0x56595559), modifier: 0x00ffffffffffffff
    'AR15'(0x35315241), modifier: 0x0000000000000000
    'AR15'(0x35315241), modifier: 0x00ffffffffffffff
    'AR12'(0x32315241), modifier: 0x0000000000000000
    'AR12'(0x32315241), modifier: 0x00ffffffffffffff
    'R8 '(0x20203852), modifier: 0x0000000000000000
    'R8 '(0x20203852), modifier: 0x00ffffffffffffff
    'GR88'(0x38385247), modifier: 0x0000000000000000
    'GR88'(0x38385247), modifier: 0x00ffffffffffffff
    'RG16'(0x36314752), modifier: 0x0000000000000000
    'RG16'(0x36314752), modifier: 0x00ffffffffffffff
    'BG24'(0x34324742), modifier: 0x920000000000001f
    'BG24'(0x34324742), modifier: 0x920000000000001e
    'BG24'(0x34324742), modifier: 0x920000000000001d
    'BG24'(0x34324742), modifier: 0x920000000000001c
    'BG24'(0x34324742), modifier: 0x920000000000001b
    'BG24'(0x34324742), modifier: 0x920000000000001a
    'BG24'(0x34324742), modifier: 0x9200000000000019
    'BG24'(0x34324742), modifier: 0x9200000000000018
    'BG24'(0x34324742), modifier: 0x0000000000000000
    'BG24'(0x34324742), modifier: 0x00ffffffffffffff
    'XB24'(0x34324258), modifier: 0x920000000000001f
    'XB24'(0x34324258), modifier: 0x920000000000001e
    'XB24'(0x34324258), modifier: 0x920000000000001d
    'XB24'(0x34324258), modifier: 0x920000000000001c
    'XB24'(0x34324258), modifier: 0x920000000000001b
    'XB24'(0x34324258), modifier: 0x920000000000001a
    'XB24'(0x34324258), modifier: 0x9200000000000019
    'XB24'(0x34324258), modifier: 0x9200000000000018
    'XB24'(0x34324258), modifier: 0x0000000000000000
    'XB24'(0x34324258), modifier: 0x00ffffffffffffff
    'XR24'(0x34325258), modifier: 0x920000000000001f
    'XR24'(0x34325258), modifier: 0x920000000000001e
    'XR24'(0x34325258), modifier: 0x920000000000001d
    'XR24'(0x34325258), modifier: 0x920000000000001c
    'XR24'(0x34325258), modifier: 0x920000000000001b
    'XR24'(0x34325258), modifier: 0x920000000000001a
    'XR24'(0x34325258), modifier: 0x9200000000000019
    'XR24'(0x34325258), modifier: 0x9200000000000018
    'XR24'(0x34325258), modifier: 0x0000000000000000
    'XR24'(0x34325258), modifier: 0x00ffffffffffffff
    'AB24'(0x34324241), modifier: 0x920000000000001f
    'AB24'(0x34324241), modifier: 0x920000000000001e
    'AB24'(0x34324241), modifier: 0x920000000000001d
    'AB24'(0x34324241), modifier: 0x920000000000001c
    'AB24'(0x34324241), modifier: 0x920000000000001b
    'AB24'(0x34324241), modifier: 0x920000000000001a
    'AB24'(0x34324241), modifier: 0x9200000000000019
    'AB24'(0x34324241), modifier: 0x9200000000000018
    'AB24'(0x34324241), modifier: 0x0000000000000000
    'AB24'(0x34324241), modifier: 0x00ffffffffffffff
    'AR24'(0x34325241), modifier: 0x920000000000001f
    'AR24'(0x34325241), modifier: 0x920000000000001e
    'AR24'(0x34325241), modifier: 0x920000000000001d
    'AR24'(0x34325241), modifier: 0x920000000000001c
    'AR24'(0x34325241), modifier: 0x920000000000001b
    'AR24'(0x34325241), modifier: 0x920000000000001a
    'AR24'(0x34325241), modifier: 0x9200000000000019
    'AR24'(0x34325241), modifier: 0x9200000000000018
    'AR24'(0x34325241), modifier: 0x0000000000000000
    'AR24'(0x34325241), modifier: 0x00ffffffffffffff
    'AB30'(0x30334241), modifier: 0x920000000000001c
    'AB30'(0x30334241), modifier: 0x9200000000000018
    'AB30'(0x30334241), modifier: 0x0000000000000000
    'AB30'(0x30334241), modifier: 0x00ffffffffffffff
    interface: 'weston_direct_display_v1', version: 1, name: 15
    interface: 'zwp_linux_explicit_synchronization_v1', version: 2, name: 16
    interface: 'weston_content_protection', version: 1, name: 17
    interface: 'wl_output', version: 3, name: 18
    x: 0, y: 0, scale: 1,
    physical_width: 0 mm, physical_height: 0 mm,
    make: 'HPN', model: 'HP Z23n G2',
    subpixel_orientation: unknown, output_transform: normal,
    mode:
    width: 800 px, height: 600 px, refresh: 60.317 Hz,
    flags: current preferred
    interface: 'zwp_input_panel_v1', version: 1, name: 19
    interface: 'zwp_input_method_v1', version: 1, name: 20
    interface: 'zwp_text_input_manager_v1', version: 1, name: 21
    interface: 'xdg_wm_base', version: 3, name: 22
    interface: 'weston_desktop_shell', version: 1, name: 23
    interface: 'weston_screenshooter', version: 1, name: 24

  • Hi T S,

    It looks like DisplayPort is hardcoded for 800x600 for SDK 9.1 and 9.2. Currently checking with the display team on this.

    Regards,

    Takuma

  • Hi T S,

    There seems to be a known issue with the DSI-2-eDP bridge on the SK-AM68 that is actively being debugged with the bridge team. The issue seems to stem from timing parameter differences where the DSI-2-eDP bridge supports reduced timing parameters instead of standard timings.

    Current plan for a fix is SDK 10.0 which should happen around July 2024 timeframe.

    Regards,

    Takuma

  • Sounds good.  WORKAROUND: Use HDMI connection instead.