This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Multiple I2S outputs on one MCASP

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: AM62P, TDA4VH, SK-AM62P-LP

Hello,

My system will have 4 externally connected speakers. Each speaker expects to get an input from an I2S bus. Is it a valid configuration to split the same MCASP clock and Frame sync to each speaker and then route a dedicated AXRx pin to each speaker? The other MCASP's on my device are used as audio inputs so I cannot dedicate an MCASP to each speaker.

I would intend to then configure ALSA to take the multichannel MCASP and "split" it into 4 outputs. I'm aware the TDA4VH SDK does not yet support MCASP but I need to work on the hardware design before the SDK is ready. Can I look at the AM62P SDK as a reference for what the TDA4VH SDK will be like?

Thanks!