This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM67: LPDDR4 ODT termination

Part Number: PROCESSOR-SDK-AM67
Other Parts Discussed in Thread: DRA829J, AM67

Hi,

In the DRA829J EVM the LPDDR4 ODT pins are pulled up to 1.1V with 10K. 

In the AM67 EVM the same ODT pins are now set at 0.55V with a 10K to 1.1V and another 10K to ground. 

Should the 10Ks to ground be removed?.

thanks