Hi,
We are looking for supporting two video Capture inputs simultaneously - VIN[0] as 24-bit and VIN[1] as 16-bit. As per the datasheet support is available for the same.
But on checking the IOMUXing of these interfaces, we found that some of the pins are conflicting with each other. Kindly let us know how we can overcome this situation and make use of two video capture input - 24-bit and 16-bit independently. The conflicting signals are given below.
Pin Number | VIN[0] 24-bit functionality | VIN[1] 18-bit functionality |
AT5 | VIN[0]A_D[16] | VIN[1]A_HSYNC |
AL5 | VIN[0]A_D[17] | VIN[1]A_VSYNC |
AK5 | VIN[0]A_D[18] | VIN[1]A_FLD |
AK4 | VIN[0]A_D[19] | VIN[1]A_DE |
Thanks & Regards,
Rohith M Ravi