Part Number: PROCESSOR-SDK-J784S4
Hi TI,
Need help regarding scaler node replication.
Scenario: I have 3 graphs.
G1 : capture1->viss1->ldc1->scaler1->........
G2: capture2->viss2->ldc2->scaler2->........
G3: scaler3-->node_x->node_y->.....
G3's first node is scaler3 node.
Goal : I want to give ldc1 and ldc2 output to the scaler3 node i.e. two input images to the scaler3 node. Both ldc1 and ldc2 outputs are objects arrays. How can I create an object array having both of these outputs to give in to scaler3.
thanks and regards,
Lalit