Other Parts Discussed in Thread: OMAP3530
I’m migrating from dsplink to syslink on a 814x. platform. The previous platform was an OMAP3530 that had dsplink configured to use only the PROC component on the HLOS. The only functionality required from dsplink was to load the DSP image, take the DSP out of reset, and read/write memory shared between the DSP and host. Consequently, the DSP code did not use dsplink at all.
It appears that the syslink ProcMgr component provides the same functionality as dsplink’s PROC component. I’m trying figure out how to configure syslink on the HLOS so that only the ProcMgr component is installed. How is this accomplished?
If only the ProcMgr is used on the HLOS, is it still necessary to configure IPC on the RTOS? If so, what component is required?