Other Parts Discussed in Thread: AM3517
Hi,
I have a few questions on the USB OTG VBUS pin:
- What is the minimum USB0_VBUS voltage that can be used with the AM3517? The USB2.0 spec indicates 4.4V in Section 7.3.2 but, with self-powered, permanently attached hub operating off 3.3V, 3.3V is much more convenient.
- If 5V is used, can the 5V be present on the AM3517 VBUS_OTG pin prior to providing AM3517 supply voltages?
- Is the VBUS valid threshold programmable?
- What is the maximum quiescent current for the USB0_VBUS pin?
Thanks,
Charlie