Part Number: AM6442
I would like to test secure boot from eMMC on AM6442 HS-SE.
Incase of "ENC_SBL_ENABLED?=yes", secure booting is succeeded.
However, secure booting in case of "ENC_ENABLED?=yes" is failed:
DMSC Firmware Version 9.1.6--v09.01.06 (Kool Koala)
DMSC Firmware revision 0x9
DMSC ABI revision 3.1
Some tests have failed!!
This log is shown if any of the using appimage are encrypted:
linux.appimage(bl31.bin, bl32.bin, u-boot-spl.bin)
hello_world.release.appimage
I referenced following question but I couldn't resolved the issue.
What else should I check to this boot issue?
my sdk:
mcu_plus_sdk_am64x_09_01_00_41
ti-processor-sdk-linux-am64xx-evm-09.01.00.08