Part Number: C6000-CGT
Hi,
I'm facing an issue with dis6x.exe, when I try to run disassembler with a cpp object file it is giving the error as follows:
$ dis6x.exe --all rbRsp_AngleEstimation.cpp.obj
Disassembly of rbRsp_AngleEstimation.cpp.obj:
INTERNAL ERROR: C:\Users\ocn2kor\ti\ti_8.3.12\bin\dis6x.exe experienced a segmentation fault
This is caused by a defect in the TI Disassembler.
TI Customer Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue".
We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Please help here.
Compiler version is C6000 v8.3.12
I tried with other disassembler llvm-dis and it is working. It is not working with TI dis6x.exe, please provide us the background for it why it is not generating any output.
Thanks,
Sairam