Part Number: PROCESSOR-SDK-AM335X
Hi,
I have installed Ubuntu 22.04.4 LTS and have installed SDK 09_01_00_001. I compile a image because I need to enable some features and Kernel (for example, CAN BUS and Bridge MAC).
For compile, I execute the command make all in <sdk-folder> and compile "without errors". I need to install three more components than setup.sh didn't install. After, install this libraries the compilation is well.
Now, I went to bin and execute create-sdcard.sh. In this program, I selected format disk /dev/sdb in two partitions and I selected option create SD card with a custom image. When the program asks me for the u-boot path. I search in the <sdk-folder> and I had found this folder <sdk-folder>/board-support/u-boot-build. In this folder I have some folders and u-boot.img and MLO.
The program continuous the normal execution and return this lines.
cp: target 'boot/MLO' is not a directory
MLO copied
cp: target 'boot/u-boot.img' is not a directory
u-boot.img copied
After, the program ask the DTB, Kernel and rootfs location.
For DTB file, I wrote the path <sdk-folder>/board-support/ti-linux-kernel-6.1.46+gitAUTOINC+ccf548983b-gccf548983b/arch/arm/boot/dts/am335x-evm.dtb.
For Kernel file, I wrote the path <sdk-folder>/board-support/ti-linux-kernel-6.1.46+gitAUTOINC+ccf548983b-gccf548983b/.
For rootfs files, I wrote the path /targetNFS/.
Is correct my locations when I create SDCard? What is the correct locations if I want to create custom image.
The location of u-boot is think is not correct because when the program ends, the /boot is empty.
Tthanks for your help,