This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure HDMI input port for OpenMax encoder component using DM8168 expansion IO Daughter board



Hi,


I am a beginner of EVM DM8168.

I am going to HDMI video input using one of the component input port( and the video source is 1920x1080p)

to test the video input port of the expansion IO Daughter card for DM8168.

I don't know how to configure hdmi input port.

I want to video capture of HDMI video input port using the expansion IO Daughter board for EVM DM8168 board.

My Ezsdk version is 5_02_01_59, but I don't clear which part should I refer to.

I test the omtb example in ezsdk, also I got some information from others about the OMX.

Please help me..

Thank you.