This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR pll clock 2 can't pass to SYSCLK10.

Dear all,

I'm developing C6A8168 Boot loader that boot from NOR Flash.

Although MAIN,DDR,VIDEO,AUDIO FAPLLs were initialized ,  SYSCLK10 couldn't get 48MHz. (It's still 27MHz)

I confirmed DDR3 clock got 800MHz. 

Why DDR pll clock2 couldn't pass to SYSCLK10 ?

 

Best regards,

 

  • Hi Kenji Sasaki,

    How are you conforming taht the DDR frequency is 800MHz?

    Could you please get these register details DDRPLL_CTRL, DDRPLL_PWD, DDRPLL_FREQ2, DDRPLL_DIV2. So that we can analize more on this.

    Thanks & Best Regards

    Anilkumar

  • Dear Anilkumar

    To check DDR3 frequency, I used Oscilloscope. (DDR0_CK0/CK0N)

    However, my oscilloscope can sample up to 5G so it might be wrong .

     

    DDRPLL_CTRL = 0x003B0188

    DDRPLL_PWD = 0x00000000

    DDRPLL_FREQ2 = 0x98D99999

    DDEPLL_DIV2 = 0x0000011E

     

    By the way, I also check freqeuncy CLKOUT line.

    CM_CLKOUT_CTRL was set 0x81.

    At this time, CLKOUT was outputting the frequency which is 27 MHz. 

    Up to reference.

     

    Best Regards

    Kenji

     

     

     

  • Hi Kenji,

    I have a quick question,

    NOR boot mode is already supported then why are you doing once again?

    Refer http://software-dl.ti.com/dsps/dsps_public_sw/psp/LinuxPSP/DM816x_04_00/04_00_00_12/index_FDS.html

     

    From the status of CM_CLKOUT_CTRL register I can say that DDR frequency is 27MHz

    I missed out one register in my earlier post, whcih is need for knowling the frequency of DDR from DDRPLL_* registers. That is "DDRPLL_DIV1"

    Regards

    Anilkumar

     ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • Hi Kenji,

    I have a quick question,

    NOR boot mode is already supported then why are you doing once again?

    Refer http://software-dl.ti.com/dsps/dsps_public_sw/psp/LinuxPSP/DM816x_04_00/04_00_00_12/index_FDS.html

     

    From the status of CM_CLKOUT_CTRL register I can say that DDR frequency is 27MHz

    I missed out one register in my earlier post, whcih is need for knowling the frequency of DDR from DDRPLL_* registers. That is "DDRPLL_DIV1"

    Regards

    Anilkumar

    ---------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------