Other Parts Discussed in Thread: TMS320DM365
Hi,
I am using embedded linux kernel with version 2.6.18 (got as a part of dvsdk_2_10_01_18 software for TMS320DM365 Target board).
In kernel source code ,in auto configuration of network devices, it is observed that a delay of about 500 msec before opening the devices and a delay of 1 sec after closing is observed for allowing the hardware registers to settle down and have a error free operation.
To have a faster operation of network devices and to have a reduction in kernel boot up time, i want to tune these pre and post delays.
Can any one tell me :
- What is the exact time to be observed before opening and after closing of the devices?
- To what lower values can these pre and post values be reduced to?
Note:
- It is observed that pre delays reduced till 100msec and post delays upto 500 msec are working fine , but further reduction in time had made the system behaviour undefined.
Thanks in advance,
Kiran.