NETRA EVM Revision E:
HDMI Port
Pin name: HDMI_EXTSWING, Pin No: AN25
Asper DM8168 Datasheet
HDMI_EXTSWING :
HDMI Voltage Reference. When HDMI is used,
this pin must be connected via an external 698-O
HDMI_EXTSWING AN25 A - - (±1% tolerance) resistor to VSS.
But the pin HDMI_EXTSWING is connected to R395 5.90K 1%.