Hi Ti Support,
I am working on AM6231 Customised board .
I made secure the Device as HS-SE using Ti Dummy keys.
After i converted into secure device its booted but for negative testcase , i tried to load bootloader images signed with other custom keys after that board is not booting.
in my device , for booting perpose i am using only DFU-USB boot method .
I am getting below issue , Please find the logs .
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
Trying to boot from MMC1
mmc_load_image_raw_sector: mmc block read error
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat: error reading image tispl.bin, err - -1
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
How to resolve this issue ?
I could not able to flash anything becuase USB is not detecting now after this logs .
Thanks,
Naresh