Part Number: SK-AM64B
Champs:
Q1.
Do we have the newest Cadence PCIE driver git?
I have browsed this git :
But it seems has no newest patch.
Q2.
Does the PCI driver we merged into the TI SDK can pass the PCIE certification?
Customer is doing 24 hours or more for the testing robustness.
But they found the PCIE will stuck someone when the PCIE is extreme busy.
Any patch / fix for the Cadence PCIE driver in the AM64 9.01 SDK is welcome.
Q3.
Please see the abnormal log attached.
There are several PCIE abnormal logs:
A. LINK DOWN!
B. pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x1000000000 64bit pref]
Those 2 abnormal logs might be related PCIE stuck while doing stress testing.
Please comment for each.
Thanks.
BR Rio
U-Boot SPL 2023.04-ga97ca328b3 (Jan 08 2024 - 08:11:13 +0000) Resetting on cold boot to workaround ErrataID:i2331 Please resend tiboot3.bin in case of UART/DFU boot resetting ... U-Boot SPL 2023.04-ga97ca328b3 (Jan 08 2024 - 08:11:13 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') SPL initial stack usage: 13384 bytes Trying to boot from MMC2 Authentication passed Authentication passed Loading Environment from MMC... *** Warning - No MMC card found, using default environment Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty NOTICE: BL31: Built : 09:34:15, Aug 24 2023 I/TC: I/TC: OP-TEE version: 4.0.0 (gcc version 11.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://urldefense.com/v3/__https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html__;!!G3vK!T95Yy-GjKgqGPGRAzmZRKOz4qogGhMNVWlZPeCM-Blyu1kptk5IicRGELPzAZwsyDCJqGH7VR6Ciog$ I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-ga97ca328b3 (Jan 08 2024 - 08:11:13 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2023.04-ga97ca328b3 (Jan 08 2024 - 08:11:13 +0000) SoC: AM64X SR2.0 HS-FS Model: Texas Instruments AM642 EVM Board: AM64-EVM rev C DRAM: 2 GiB Core: 66 devices, 31 uclasses, devicetree: separate NAND: 0 MiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Unidentified board claims AM64-EVM in eeprom header Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 574 bytes read in 30 ms (18.6 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... ## Error: "main_cpsw0_qsgmii_phyinit" not defined 20836864 bytes read in 893 ms (22.3 MiB/s) 59008 bytes read in 34 ms (1.7 MiB/s) Working FDT set to 88000000 ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Working FDT set to 88000000 Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK Working FDT set to 8feee000 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.1.69 (wade@n0name) (aarch64-linux-gnu-gcc (GCC) 11.3.1 20220604 [releases/gcc-11 revision 591c0f4b92548e3ae2e8173f4f93984b1c7f62bb], GNU ld (Linaro_Binutils-2022.06) 2.37.20220122) #6 SMP PREEMPT Tue Apr 9 15:17:29 CST 2024 [ 0.000000] Machine model: Texas Instruments AM642 EVM [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a57fffff] [ 0.000000] node 0: [mem 0x00000000a5800000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] cma: Reserved 32 MiB at 0x00000000fba00000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.4 [ 0.000000] percpu: Embedded 19 pages/cpu s38056 r8192 d31576 u77824 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] alternatives: applying boot alternatives [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=56bb290c-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1888632K/2097152K available (12800K kernel code, 1276K rwdata, 4020K rodata, 2112K init, 447K bss, 175752K reserved, 32768K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] Root IRQ handler: gic_handle_irq [ 0.000000] GICv3: GICv3 features: 16 PPIs [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000080030000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000 [ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention. [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008610] Console: colour dummy device 80x25 [ 0.013212] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023894] pid_max: default: 32768 minimum: 301 [ 0.028674] LSM: Security Framework initializing [ 0.033549] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.041131] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.051084] cblist_init_generic: Setting adjustable number of callback queues. [ 0.058546] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.064853] cblist_init_generic: Setting adjustable number of callback queues. [ 0.072246] cblist_init_generic: Setting shift to 1 and lim to 1. [ 0.078658] rcu: Hierarchical SRCU implementation. [ 0.083568] rcu: Max phase no-delay instances is 1000. [ 0.089215] Platform MSI: msi-controller@1820000 domain created [ 0.095582] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.105080] EFI services will not be available. [ 0.110025] smp: Bringing up secondary CPUs ... I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot [ 0.123696] Detected VIPT I-cache on CPU1 [ 0.123837] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000 [ 0.123859] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000 [ 0.123921] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.124052] smp: Brought up 1 node, 2 CPUs [ 0.153441] SMP: Total of 2 processors activated. [ 0.158254] CPU features: detected: 32-bit EL0 Support [ 0.163523] CPU features: detected: CRC32 instructions [ 0.168842] CPU: All CPU(s) started at EL2 [ 0.173027] alternatives: applying system-wide alternatives [ 0.180700] devtmpfs: initialized [ 0.193873] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.203889] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.212230] pinctrl core: initialized pinctrl subsystem [ 0.218303] DMI not present or invalid. [ 0.223026] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.230411] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.237879] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.245997] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.254206] audit: initializing netlink subsys (disabled) [ 0.260111] audit: type=2000 audit(0.164:1): state=initialized audit_enabled=0 res=1 [ 0.260737] thermal_sys: Registered thermal governor 'step_wise' [ 0.268047] thermal_sys: Registered thermal governor 'power_allocator' [ 0.274456] cpuidle: using governor menu [ 0.285392] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.292405] ASID allocator initialised with 65536 entries [ 0.306988] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@f4000/pinctrl@a40000/cpsw-cpts-pps [ 0.321521] KASLR disabled due to lack of seed [ 0.334604] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages [ 0.341575] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.347985] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages [ 0.354922] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.361328] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages [ 0.368262] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.374667] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages [ 0.381604] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 0.389872] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3802f] Detected [ 0.400490] iommu: Default domain type: Translated [ 0.405494] iommu: DMA domain TLB invalidation policy: strict mode [ 0.412262] SCSI subsystem initialized [ 0.416598] usbcore: registered new interface driver usbfs [ 0.422263] usbcore: registered new interface driver hub [ 0.427730] usbcore: registered new device driver usb [ 0.433427] pps_core: LinuxPPS API ver. 1 registered [ 0.438510] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.447857] PTP clock support registered [ 0.452009] EDAC MC: Ver: 3.0.0 [ 0.456491] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100 [ 0.463457] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100 [ 0.470301] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100 [ 0.477582] FPGA manager framework [ 0.481197] Advanced Linux Sound Architecture Driver Initialized. [ 0.488664] clocksource: Switched to clocksource arch_sys_counter [ 0.495248] VFS: Disk quotas dquot_6.6.0 [ 0.499326] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.513541] NET: Registered PF_INET protocol family [ 0.518874] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.528560] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.537407] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.545356] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.553582] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear) [ 0.561624] TCP: Hash tables configured (established 16384 bind 16384) [ 0.568578] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.575524] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.583148] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.589547] RPC: Registered named UNIX socket transport module. [ 0.595655] RPC: Registered udp transport module. [ 0.600466] RPC: Registered tcp transport module. [ 0.605275] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.611864] NET: Registered PF_XDP protocol family [ 0.616805] PCI: CLS 0 bytes, default 64 [ 0.621669] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.631882] Initialise system trusted keyrings [ 0.636848] workingset: timestamp_bits=46 max_order=19 bucket_order=0 [ 0.648819] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.655598] NFS: Registering the id_resolver key type [ 0.660860] Key type id_resolver registered [ 0.665142] Key type id_legacy registered [ 0.669304] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.676162] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.727035] Key type asymmetric registered [ 0.731240] Asymmetric key parser 'x509' registered [ 0.736294] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.744119] io scheduler mq-deadline registered [ 0.748766] io scheduler kyber registered [ 0.756482] pinctrl-single 4084000.pinctrl: 33 pins, size 132 [ 0.763039] pinctrl-single f4000.pinctrl: 180 pins, size 720 [ 0.770681] pinctrl-single a40000.pinctrl: 512 pins, size 2048 [ 0.783383] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled [ 0.801159] loop: module loaded [ 0.805701] megasas: 07.719.03.00-rc1 [ 0.813376] tun: Universal TUN/TAP device driver, 1.6 [ 0.819479] thunder_xcv, ver 1.0 [ 0.822859] thunder_bgx, ver 1.0 [ 0.826201] nicpf, ver 1.0 [ 0.829151] e1000: Intel(R) PRO/1000 Network Driver [ 0.834139] e1000: Copyright (c) 1999-2006 Intel Corporation. [ 0.840063] e1000e: Intel(R) PRO/1000 Network Driver [ 0.845137] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 0.851230] igb: Intel(R) Gigabit Ethernet Network Driver [ 0.856748] igb: Copyright (c) 2007-2014 Intel Corporation. [ 0.862483] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.868889] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.875094] sky2: driver version 1.30 [ 0.879720] VFIO - User Level meta-driver version: 0.3 [ 0.886031] usbcore: registered new interface driver usb-storage [ 0.893000] i2c_dev: i2c /dev entries driver [ 0.898545] sdhci: Secure Digital Host Controller Interface driver [ 0.904903] sdhci: Copyright(c) Pierre Ossman [ 0.909590] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.916127] ledtrig-cpu: registered to indicate activity on CPUs [ 0.922514] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.929486] usbcore: registered new interface driver usbhid [ 0.935197] usbhid: USB HID core driver [ 0.940216] optee: probing for conduit method. I/TC: Reserved shared memory is enabled I/TC: Dynamic shared memory is enabled I/TC: Normal World virtualization support is disabled I/TC: Asynchronous notifications are disabled [ 0.944853] optee: revision 4.0 (2a5b1d12) [ 0.961510] optee: dynamic shared memory is enabled [ 0.971183] optee: initialized driver [ 0.977344] ipip: IPv4 and MPLS over IPv4 tunneling driver [ 0.983497] Initializing XFRM netlink socket [ 0.988302] NET: Registered PF_INET6 protocol family [ 0.994926] Segment Routing with IPv6 [ 0.998768] In-situ OAM (IOAM) with IPv6 [ 1.002898] mip6: Mobile IPv6 [ 1.005936] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.013128] NET: Registered PF_PACKET protocol family [ 1.018378] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. [ 1.031708] Key type dns_resolver registered [ 1.036681] registered taskstats version 1 [ 1.040904] Loading compiled-in X.509 certificates [ 1.057917] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') [ 1.103521] pca953x 0-0022: supply vcc not found, using dummy regulator [ 1.110497] pca953x 0-0022: using AI [ 1.137994] omap_i2c 20010000.i2c: bus 0 rev0.12 at 400 kHz [ 1.144240] ti-sci-intr bus@f4000:interrupt-controller@a00000: Interrupt Router 3 domain created [ 1.153648] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 1.165801] ti-udma 485c0100.dma-controller: Number of rings: 68 [ 1.173419] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6) [ 1.183582] ti-udma 485c0000.dma-controller: Number of rings: 288 [ 1.198876] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15) [ 1.209942] printk: console [ttyS2] disabled [ 1.214416] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 304, base_baud = 3000000) is a 8250 [ 1.223308] printk: console [ttyS2] enabled [ 1.223308] printk: console [ttyS2] enabled [ 1.231766] printk: bootconsole [ns16550a0] disabled [ 1.231766] printk: bootconsole [ns16550a0] disabled [ 1.246527] spi-nor spi0.0: s28hs512t (65536 Kbytes) [ 1.251658] 7 fixed-partitions partitions found on MTD device fc40000.spi.0 [ 1.258637] Creating 7 MTD partitions on "fc40000.spi.0": [ 1.264034] 0x000000000000-0x000000100000 : "ospi.tiboot3" [ 1.271007] 0x000000100000-0x000000300000 : "ospi.tispl" [ 1.277736] 0x000000300000-0x000000700000 : "ospi.u-boot" [ 1.284559] 0x000000700000-0x000000740000 : "ospi.env" [ 1.291150] 0x000000740000-0x000000780000 : "ospi.env.backup" [ 1.298283] 0x000000800000-0x000003fc0000 : "ospi.rootfs" [ 1.305142] 0x000003fc0000-0x000004000000 : "ospi.phypattern" [ 1.321511] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.364705] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.374022] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867 [ 1.382197] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006 [ 1.395114] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4 [ 1.402254] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [ 1.409033] pps pps0: new PPS source ptp0 [ 1.413469] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1 [ 1.424283] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16 [ 1.435559] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0 [ 1.445954] mmc0: CQHCI version 5.10 [ 1.451212] gpio-mux mux-controller: 2-way mux-controller registered [ 1.468621] Rio_debug j721e_pcie_probe enter [ 1.472987] j721e-pcie-host f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges: [ 1.480874] j721e-pcie-host f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000 [ 1.489409] j721e-pcie-host f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000 [ 1.491318] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [ 1.497981] j721e-pcie-host f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000 [ 1.513972] Rio_debug: j721e_pcie_common_init --entered [ 1.519253] Rio_debug: j721e_pcie_ctrl_init --entered [ 1.524310] Rio_debug: j721e_pcie_set_mode --entered [ 1.529321] Rio_debug: j721e_pcie_set_link_speed --entered [ 1.534820] Rio_debug: j721e_pcie_set_lane_count --entered [ 1.540300] Rio_debug: j721e_pcie_setup_link_interrupts --entered [ 1.546571] Rio_debug: j721e_pcie_config_link_irq --entered [ 1.552139] Rio_debug j721e_pcie_config_legacy_irq enter [ 1.557541] Rio_debug j721e_enable_acspcie enter [ 1.566005] Rio_debug cdns_pcie_host_setup enter [ 1.570695] Rio_debug cdns_pcie_host_enable_ptm_response enter [ 1.576525] Rio_debug: j721e_pcie_start_link --entered [ 1.581655] Rio_debug cdns_pcie_host_start_link enter [ 1.586697] Rio_debug cdns_pcie_host_wait_for_link enter [ 1.592013] Rio_debug: j721e_pcie_link_up --entered [ 1.592247] mmc0: Command Queue Engine enabled [ 1.596895] Link up [ 1.596898] Rio_debug cdns_pcie_host_init enter [ 1.596901] Rio_debug cdns_pcie_host_init_root_port enter [ 1.596907] Rio_debug cdns_pcie_host_init_address_translation enter [ 1.596918] Rio_debug cdns_pcie_host_map_dma_ranges enter [ 1.601364] mmc0: new HS200 MMC card at address 0001 [ 1.603431] Rio_debug cdns_pcie_host_bar_config enter [ 1.608826] mmcblk0: mmc0:0001 S0J56X 14.8 GiB [ 1.613366] Rio_debug cdns_pcie_host_find_min_bar enter [ 1.621726] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB [ 1.625010] Rio_debug cdns_pcie_host_bar_ib_config enter [ 1.625221] j721e-pcie-host f102000.pcie: PCI host bridge to bus 0000:00 [ 1.631350] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB [ 1.635064] pci_bus 0000:00: root bus resource [bus 00-ff] [ 1.640775] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (240:0) [ 1.644809] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x68001000-0x68010fff]) [ 1.644821] pci_bus 0000:00: root bus resource [mem 0x68011000-0x6fffffff] [ 1.644835] Rio_debug cdns_pci_map_bus enter [ 1.699001] Rio_debug cdns_pci_map_bus enter [ 1.703268] Rio_debug cdns_pci_map_bus enter [ 1.707533] Rio_debug cdns_pci_map_bus enter [ 1.711798] Rio_debug cdns_pci_map_bus enter [ 1.716062] Rio_debug cdns_pci_map_bus enter [ 1.720333] Rio_debug cdns_pci_map_bus enter [ 1.724597] Rio_debug cdns_pci_map_bus enter [ 1.728860] Rio_debug cdns_pci_map_bus enter [ 1.733124] Rio_debug cdns_pci_map_bus enter [ 1.737402] Rio_debug cdns_pci_map_bus enter [ 1.741666] Rio_debug cdns_pci_map_bus enter [ 1.745930] Rio_debug cdns_pci_map_bus enter [ 1.750194] Rio_debug cdns_pci_map_bus enter [ 1.754466] pci 0000:00:00.0: [104c:b010] type 01 class 0x060400 [ 1.760474] Rio_debug cdns_pci_map_bus enter [ 1.764740] Rio_debug cdns_pci_map_bus enter [ 1.769004] Rio_debug cdns_pci_map_bus enter [ 1.773330] Rio_debug cdns_pci_map_bus enter [ 1.777615] Rio_debug cdns_pci_map_bus enter [ 1.781880] Rio_debug cdns_pci_map_bus enter [ 1.786144] Rio_debug cdns_pci_map_bus enter [ 1.790408] Rio_debug cdns_pci_map_bus enter [ 1.794671] Rio_debug cdns_pci_map_bus enter [ 1.798935] Rio_debug cdns_pci_map_bus enter [ 1.803199] Rio_debug cdns_pci_map_bus enter [ 1.807462] Rio_debug cdns_pci_map_bus enter [ 1.811725] Rio_debug cdns_pci_map_bus enter [ 1.815990] Rio_debug cdns_pci_map_bus enter [ 1.820257] Rio_debug cdns_pci_map_bus enter [ 1.824526] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0xfffffffff 64bit pref] [ 1.831834] Rio_debug cdns_pci_map_bus enter [ 1.836096] Rio_debug cdns_pci_map_bus enter [ 1.840360] Rio_debug cdns_pci_map_bus enter [ 1.844624] Rio_debug cdns_pci_map_bus enter [ 1.848907] Rio_debug cdns_pci_map_bus enter [ 1.853182] Rio_debug cdns_pci_map_bus enter [ 1.857448] Rio_debug cdns_pci_map_bus enter [ 1.861712] Rio_debug cdns_pci_map_bus enter [ 1.865976] Rio_debug cdns_pci_map_bus enter [ 1.870240] Rio_debug cdns_pci_map_bus enter [ 1.874504] Rio_debug cdns_pci_map_bus enter [ 1.878772] Rio_debug cdns_pci_map_bus enter [ 1.883037] Rio_debug cdns_pci_map_bus enter [ 1.887300] Rio_debug cdns_pci_map_bus enter [ 1.891564] Rio_debug cdns_pci_map_bus enter [ 1.895826] Rio_debug cdns_pci_map_bus enter [ 1.900090] Rio_debug cdns_pci_map_bus enter [ 1.904352] Rio_debug cdns_pci_map_bus enter [ 1.908616] Rio_debug cdns_pci_map_bus enter [ 1.912881] Rio_debug cdns_pci_map_bus enter [ 1.917147] Rio_debug cdns_pci_map_bus enter [ 1.921412] Rio_debug cdns_pci_map_bus enter [ 1.925678] Rio_debug cdns_pci_map_bus enter [ 1.929943] Rio_debug cdns_pci_map_bus enter [ 1.934206] Rio_debug cdns_pci_map_bus enter [ 1.938474] Rio_debug cdns_pci_map_bus enter [ 1.942737] Rio_debug cdns_pci_map_bus enter [ 1.947001] Rio_debug cdns_pci_map_bus enter [ 1.951266] Rio_debug cdns_pci_map_bus enter [ 1.955528] Rio_debug cdns_pci_map_bus enter [ 1.959791] Rio_debug cdns_pci_map_bus enter [ 1.964056] Rio_debug cdns_pci_map_bus enter [ 1.968328] Rio_debug cdns_pci_map_bus enter [ 1.972613] Rio_debug cdns_pci_map_bus enter [ 1.976877] Rio_debug cdns_pci_map_bus enter [ 1.981141] Rio_debug cdns_pci_map_bus enter [ 1.985404] Rio_debug cdns_pci_map_bus enter [ 1.989666] Rio_debug cdns_pci_map_bus enter [ 1.993931] Rio_debug cdns_pci_map_bus enter [ 1.998200] Rio_debug cdns_pci_map_bus enter [ 2.002464] Rio_debug cdns_pci_map_bus enter [ 2.006728] Rio_debug cdns_pci_map_bus enter [ 2.010992] Rio_debug cdns_pci_map_bus enter [ 2.015255] Rio_debug cdns_pci_map_bus enter [ 2.019519] Rio_debug cdns_pci_map_bus enter [ 2.023781] Rio_debug cdns_pci_map_bus enter [ 2.028044] Rio_debug cdns_pci_map_bus enter [ 2.032309] Rio_debug cdns_pci_map_bus enter [ 2.036573] Rio_debug cdns_pci_map_bus enter [ 2.040837] Rio_debug cdns_pci_map_bus enter [ 2.045100] Rio_debug cdns_pci_map_bus enter [ 2.049364] Rio_debug cdns_pci_map_bus enter [ 2.053626] Rio_debug cdns_pci_map_bus enter [ 2.057894] Rio_debug cdns_pci_map_bus enter [ 2.062159] Rio_debug cdns_pci_map_bus enter [ 2.066423] Rio_debug cdns_pci_map_bus enter [ 2.070689] Rio_debug cdns_pci_map_bus enter [ 2.074951] Rio_debug cdns_pci_map_bus enter [ 2.079213] Rio_debug cdns_pci_map_bus enter [ 2.083476] Rio_debug cdns_pci_map_bus enter [ 2.087738] Rio_debug cdns_pci_map_bus enter [ 2.092001] Rio_debug cdns_pci_map_bus enter [ 2.096265] Rio_debug cdns_pci_map_bus enter [ 2.100527] Rio_debug cdns_pci_map_bus enter [ 2.104791] Rio_debug cdns_pci_map_bus enter [ 2.109053] Rio_debug cdns_pci_map_bus enter [ 2.113316] Rio_debug cdns_pci_map_bus enter [ 2.117582] Rio_debug cdns_pci_map_bus enter [ 2.121846] Rio_debug cdns_pci_map_bus enter [ 2.126108] Rio_debug cdns_pci_map_bus enter [ 2.130371] Rio_debug cdns_pci_map_bus enter [ 2.134637] Rio_debug cdns_pci_map_bus enter [ 2.138899] Rio_debug cdns_pci_map_bus enter [ 2.143164] Rio_debug cdns_pci_map_bus enter [ 2.147428] Rio_debug cdns_pci_map_bus enter [ 2.151692] Rio_debug cdns_pci_map_bus enter [ 2.155956] Rio_debug cdns_pci_map_bus enter [ 2.160219] Rio_debug cdns_pci_map_bus enter [ 2.164482] Rio_debug cdns_pci_map_bus enter [ 2.168744] Rio_debug cdns_pci_map_bus enter [ 2.173008] Rio_debug cdns_pci_map_bus enter [ 2.177275] Rio_debug cdns_pci_map_bus enter [ 2.181539] Rio_debug cdns_pci_map_bus enter [ 2.185803] Rio_debug cdns_pci_map_bus enter [ 2.190065] Rio_debug cdns_pci_map_bus enter [ 2.194327] Rio_debug cdns_pci_map_bus enter [ 2.198591] Rio_debug cdns_pci_map_bus enter [ 2.202854] Rio_debug cdns_pci_map_bus enter [ 2.207118] Rio_debug cdns_pci_map_bus enter [ 2.211381] Rio_debug cdns_pci_map_bus enter [ 2.215643] Rio_debug cdns_pci_map_bus enter [ 2.219905] Rio_debug cdns_pci_map_bus enter [ 2.224173] Rio_debug cdns_pci_map_bus enter [ 2.228437] Rio_debug cdns_pci_map_bus enter [ 2.232701] Rio_debug cdns_pci_map_bus enter [ 2.236972] Rio_debug cdns_pci_map_bus enter [ 2.241241] pci 0000:00:00.0: supports D1 [ 2.245249] pci 0000:00:00.0: PME# supported from D0 D1 D3hot [ 2.250990] Rio_debug cdns_pci_map_bus enter [ 2.255252] Rio_debug cdns_pci_map_bus enter [ 2.259517] Rio_debug cdns_pci_map_bus enter [ 2.263780] Rio_debug cdns_pci_map_bus enter [ 2.268043] Rio_debug cdns_pci_map_bus enter [ 2.272305] Rio_debug cdns_pci_map_bus enter [ 2.276569] Rio_debug cdns_pci_map_bus enter [ 2.280833] Rio_debug cdns_pci_map_bus enter [ 2.285095] Rio_debug cdns_pci_map_bus enter [ 2.289358] Rio_debug cdns_pci_map_bus enter [ 2.293622] Rio_debug cdns_pci_map_bus enter [ 2.297891] Rio_debug cdns_pci_map_bus enter [ 2.302156] Rio_debug cdns_pci_map_bus enter [ 2.306419] Rio_debug cdns_pci_map_bus enter [ 2.310683] Rio_debug cdns_pci_map_bus enter [ 2.314948] Rio_debug cdns_pci_map_bus enter [ 2.319211] Rio_debug cdns_pci_map_bus enter [ 2.323474] Rio_debug cdns_pci_map_bus enter [ 2.327736] Rio_debug cdns_pci_map_bus enter [ 2.331999] Rio_debug cdns_pci_map_bus enter [ 2.336261] Rio_debug cdns_pci_map_bus enter [ 2.340525] Rio_debug cdns_pci_map_bus enter [ 2.344791] Rio_debug cdns_pci_map_bus enter [ 2.349053] Rio_debug cdns_pci_map_bus enter [ 2.353316] Rio_debug cdns_pci_map_bus enter [ 2.357584] Rio_debug cdns_pci_map_bus enter [ 2.361847] Rio_debug cdns_pci_map_bus enter [ 2.366111] Rio_debug cdns_pci_map_bus enter [ 2.370374] Rio_debug cdns_pci_map_bus enter [ 2.374636] Rio_debug cdns_pci_map_bus enter [ 2.378898] Rio_debug cdns_pci_map_bus enter [ 2.383161] Rio_debug cdns_pci_map_bus enter [ 2.387423] Rio_debug cdns_pci_map_bus enter [ 2.391687] Rio_debug cdns_pci_map_bus enter [ 2.395956] Rio_debug cdns_pci_map_bus enter [ 2.400223] Rio_debug cdns_pci_map_bus enter [ 2.404486] Rio_debug cdns_pci_map_bus enter [ 2.408750] Rio_debug cdns_pci_map_bus enter [ 2.413012] Rio_debug cdns_pci_map_bus enter [ 2.417279] Rio_debug cdns_pci_map_bus enter [ 2.421544] Rio_debug cdns_pci_map_bus enter [ 2.425808] Rio_debug cdns_pci_map_bus enter [ 2.430072] Rio_debug cdns_pci_map_bus enter [ 2.434338] Rio_debug cdns_pci_map_bus enter [ 2.438602] Rio_debug cdns_pci_map_bus enter [ 2.442865] Rio_debug cdns_pci_map_bus enter [ 2.447128] Rio_debug cdns_pci_map_bus enter [ 2.451394] Rio_debug cdns_pci_map_bus enter [ 2.455657] Rio_debug cdns_pci_map_bus enter [ 2.459922] Rio_debug cdns_pci_map_bus enter [ 2.464350] Rio_debug cdns_pci_map_bus enter [ 2.468616] Rio_debug cdns_pci_map_bus enter [ 2.472880] Rio_debug cdns_pci_map_bus enter [ 2.477149] Rio_debug cdns_pci_map_bus enter [ 2.481413] Rio_debug cdns_pci_map_bus enter [ 2.485676] Rio_debug cdns_pci_map_bus enter [ 2.489941] Rio_debug cdns_pci_map_bus enter [ 2.494202] Rio_debug cdns_pci_map_bus enter [ 2.498466] Rio_debug cdns_pci_map_bus enter [ 2.502730] Rio_debug cdns_pci_map_bus enter [ 2.506993] Rio_debug cdns_pci_map_bus enter [ 2.511256] Rio_debug cdns_pci_map_bus enter [ 2.515520] Rio_debug cdns_pci_map_bus enter [ 2.519784] Rio_debug cdns_pci_map_bus enter [ 2.524048] Rio_debug cdns_pci_map_bus enter [ 2.528312] Rio_debug cdns_pci_map_bus enter [ 2.532574] Rio_debug cdns_pci_map_bus enter [ 2.536841] Rio_debug cdns_pci_map_bus enter [ 2.541106] Rio_debug cdns_pci_map_bus enter [ 2.545369] Rio_debug cdns_pci_map_bus enter [ 2.549632] Rio_debug cdns_pci_map_bus enter [ 2.553898] Rio_debug cdns_pci_map_bus enter [ 2.558161] Rio_debug cdns_pci_map_bus enter [ 2.562425] Rio_debug cdns_pci_map_bus enter [ 2.566688] Rio_debug cdns_pci_map_bus enter [ 2.570952] Rio_debug cdns_pci_map_bus enter [ 2.575216] Rio_debug cdns_pci_map_bus enter [ 2.579480] Rio_debug cdns_pci_map_bus enter [ 2.583742] Rio_debug cdns_pci_map_bus enter [ 2.588004] Rio_debug cdns_pci_map_bus enter [ 2.592268] Rio_debug cdns_pci_map_bus enter [ 2.596532] Rio_debug cdns_pci_map_bus enter [ 2.600799] Rio_debug cdns_pci_map_bus enter [ 2.605064] Rio_debug cdns_pci_map_bus enter [ 2.609326] Rio_debug cdns_pci_map_bus enter [ 2.613589] Rio_debug cdns_pci_map_bus enter [ 2.617960] Rio_debug cdns_pci_map_bus enter [ 2.622511] Rio_debug cdns_pci_map_bus enter [ 2.626907] Rio_debug cdns_pci_map_bus enter [ 2.631244] Rio_debug cdns_pci_map_bus enter [ 2.635578] Rio_debug cdns_pci_map_bus enter [ 2.639910] Rio_debug cdns_pci_map_bus enter [ 2.644242] Rio_debug cdns_pci_map_bus enter [ 2.648575] Rio_debug cdns_pci_map_bus enter [ 2.652906] Rio_debug cdns_pci_map_bus enter [ 2.657244] Rio_debug cdns_pci_map_bus enter [ 2.661594] Rio_debug cdns_pci_map_bus enter [ 2.665927] Rio_debug cdns_pci_map_bus enter [ 2.670259] Rio_debug cdns_pci_map_bus enter [ 2.674591] Rio_debug cdns_pci_map_bus enter [ 2.678924] Rio_debug cdns_pci_map_bus enter [ 2.683257] Rio_debug cdns_pci_map_bus enter [ 2.687590] Rio_debug cdns_pci_map_bus enter [ 2.691921] Rio_debug cdns_pci_map_bus enter [ 2.696251] Rio_debug cdns_pci_map_bus enter [ 2.700584] Rio_debug cdns_pci_map_bus enter [ 2.704914] Rio_debug cdns_pci_map_bus enter [ 2.709245] Rio_debug cdns_pci_map_bus enter [ 2.713577] Rio_debug cdns_pci_map_bus enter [ 2.717908] Rio_debug cdns_pci_map_bus enter [ 2.722249] Rio_debug cdns_pci_map_bus enter [ 2.726582] Rio_debug cdns_pci_map_bus enter [ 2.730914] Rio_debug cdns_pci_map_bus enter [ 2.735247] Rio_debug cdns_pci_map_bus enter [ 2.739672] Rio_debug cdns_pci_map_bus enter [ 2.744078] Rio_debug cdns_pci_map_bus enter [ 2.748432] Rio_debug cdns_pci_map_bus enter [ 2.752774] Rio_debug cdns_pci_map_bus enter [ 2.757045] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring [ 2.765049] Rio_debug cdns_pci_map_bus enter [ 2.769313] Rio_debug cdns_pci_map_bus enter [ 2.773578] Rio_debug cdns_pci_map_bus enter [ 2.777846] Rio_debug cdns_pci_map_bus enter [ 2.782119] Rio_debug cdns_pci_map_bus enter [ 2.786384] Rio_debug cdns_pci_map_bus enter [ 2.790649] Rio_debug cdns_pci_map_bus enter [ 2.794912] Rio_debug cdns_pci_map_bus enter [ 2.799174] Rio_debug cdns_pci_map_bus enter [ 2.803438] Rio_debug cdns_pci_map_bus enter [ 2.807703] Rio_debug cdns_pci_map_bus enter [ 2.811968] Rio_debug cdns_pci_map_bus enter [ 2.816286] Rio_debug cdns_pci_map_bus enter [ 2.820576] Rio_debug cdns_pci_map_bus enter [ 2.824841] Rio_debug cdns_pci_map_bus enter [ 2.829104] Rio_debug cdns_pci_map_bus enter [ 2.833383] Rio_debug cdns_pci_map_bus enter [ 2.837647] Rio_debug cdns_pci_map_bus enter [ 2.841917] Rio_debug cdns_pci_map_bus enter [ 2.846180] Rio_debug cdns_pci_map_bus enter [ 2.850443] Rio_debug cdns_pci_map_bus enter [ 2.854706] Rio_debug cdns_pci_map_bus enter [ 2.858968] Rio_debug cdns_pci_map_bus enter [ 2.863231] Rio_debug cdns_pci_map_bus enter [ 2.867493] Rio_debug cdns_pci_map_bus enter [ 2.871760] Rio_debug cdns_pci_map_bus enter [ 2.876023] Rio_debug cdns_pci_map_bus enter [ 2.880286] Rio_debug cdns_pci_map_bus enter [ 2.884549] Rio_debug cdns_pci_map_bus enter [ 2.888812] Rio_debug cdns_pci_map_bus enter [ 2.893074] Rio_debug cdns_pci_map_bus enter [ 2.897336] Rio_debug cdns_pci_map_bus enter [ 2.901603] Rio_debug cdns_pci_map_bus enter [ 2.905867] Rio_debug cdns_pci_map_bus enter [ 2.910131] Rio_debug cdns_pci_map_bus enter [ 2.914394] Rio_debug cdns_pci_map_bus enter [ 2.918786] Rio_debug cdns_pci_map_bus enter [ 2.923055] Rio_debug cdns_pci_map_bus enter [ 2.927324] Rio_debug cdns_pci_map_bus enter [ 2.931591] Rio_debug cdns_pci_map_bus enter [ 2.935857] Rio_debug cdns_pci_map_bus enter [ 2.940123] Rio_debug cdns_pci_map_bus enter [ 2.944387] Rio_debug cdns_pci_map_bus enter [ 2.948653] Rio_debug cdns_pci_map_bus enter [ 2.952918] Rio_debug cdns_pci_map_bus enter [ 2.957184] Rio_debug cdns_pci_map_bus enter [ 2.961488] Rio_debug cdns_pci_map_bus enter [ 2.965758] Rio_debug cdns_pci_map_bus enter [ 2.970025] Rio_debug cdns_pci_map_bus enter [ 2.974294] Rio_debug cdns_pci_map_bus enter [ 2.978568] pci 0000:01:00.0: [13a8:0358] type 00 class 0x070002 [ 2.984572] Rio_debug cdns_pci_map_bus enter [ 2.988839] Rio_debug cdns_pci_map_bus enter [ 2.993105] Rio_debug cdns_pci_map_bus enter [ 2.997370] Rio_debug cdns_pci_map_bus enter [ 3.001635] Rio_debug cdns_pci_map_bus enter [ 3.005900] Rio_debug cdns_pci_map_bus enter [ 3.010167] Rio_debug cdns_pci_map_bus enter [ 3.014432] Rio_debug cdns_pci_map_bus enter [ 3.018696] Rio_debug cdns_pci_map_bus enter [ 3.022965] Rio_debug cdns_pci_map_bus enter [ 3.027232] Rio_debug cdns_pci_map_bus enter [ 3.031503] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x00003fff] [ 3.037768] Rio_debug cdns_pci_map_bus enter [ 3.042033] Rio_debug cdns_pci_map_bus enter [ 3.046299] Rio_debug cdns_pci_map_bus enter [ 3.050563] Rio_debug cdns_pci_map_bus enter [ 3.054828] Rio_debug cdns_pci_map_bus enter [ 3.059126] Rio_debug cdns_pci_map_bus enter [ 3.063410] Rio_debug cdns_pci_map_bus enter [ 3.067676] Rio_debug cdns_pci_map_bus enter [ 3.071942] Rio_debug cdns_pci_map_bus enter [ 3.076207] Rio_debug cdns_pci_map_bus enter [ 3.080476] Rio_debug cdns_pci_map_bus enter [ 3.084746] Rio_debug cdns_pci_map_bus enter [ 3.089012] Rio_debug cdns_pci_map_bus enter [ 3.093276] Rio_debug cdns_pci_map_bus enter [ 3.097541] Rio_debug cdns_pci_map_bus enter [ 3.101809] Rio_debug cdns_pci_map_bus enter [ 3.106075] Rio_debug cdns_pci_map_bus enter [ 3.110341] Rio_debug cdns_pci_map_bus enter [ 3.114607] Rio_debug cdns_pci_map_bus enter [ 3.118872] Rio_debug cdns_pci_map_bus enter [ 3.123136] Rio_debug cdns_pci_map_bus enter [ 3.127403] Rio_debug cdns_pci_map_bus enter [ 3.131667] Rio_debug cdns_pci_map_bus enter [ 3.135950] Rio_debug cdns_pci_map_bus enter [ 3.140227] Rio_debug cdns_pci_map_bus enter [ 3.144494] Rio_debug cdns_pci_map_bus enter [ 3.148765] Rio_debug cdns_pci_map_bus enter [ 3.153033] Rio_debug cdns_pci_map_bus enter [ 3.157297] Rio_debug cdns_pci_map_bus enter [ 3.161562] Rio_debug cdns_pci_map_bus enter [ 3.165827] Rio_debug cdns_pci_map_bus enter [ 3.170092] Rio_debug cdns_pci_map_bus enter [ 3.174361] Rio_debug cdns_pci_map_bus enter [ 3.178627] Rio_debug cdns_pci_map_bus enter [ 3.182895] Rio_debug cdns_pci_map_bus enter [ 3.187161] Rio_debug cdns_pci_map_bus enter [ 3.191428] Rio_debug cdns_pci_map_bus enter [ 3.195695] Rio_debug cdns_pci_map_bus enter [ 3.199961] Rio_debug cdns_pci_map_bus enter [ 3.204233] Rio_debug cdns_pci_map_bus enter [ 3.208498] Rio_debug cdns_pci_map_bus enter [ 3.212767] Rio_debug cdns_pci_map_bus enter [ 3.217034] Rio_debug cdns_pci_map_bus enter [ 3.221300] Rio_debug cdns_pci_map_bus enter [ 3.225565] Rio_debug cdns_pci_map_bus enter [ 3.229831] Rio_debug cdns_pci_map_bus enter [ 3.234096] Rio_debug cdns_pci_map_bus enter [ 3.238360] Rio_debug cdns_pci_map_bus enter [ 3.242625] Rio_debug cdns_pci_map_bus enter [ 3.246891] Rio_debug cdns_pci_map_bus enter [ 3.251156] Rio_debug cdns_pci_map_bus enter [ 3.255420] Rio_debug cdns_pci_map_bus enter [ 3.259686] Rio_debug cdns_pci_map_bus enter [ 3.263953] Rio_debug cdns_pci_map_bus enter [ 3.268219] Rio_debug cdns_pci_map_bus enter [ 3.272484] Rio_debug cdns_pci_map_bus enter [ 3.276752] Rio_debug cdns_pci_map_bus enter [ 3.281018] Rio_debug cdns_pci_map_bus enter [ 3.285288] Rio_debug cdns_pci_map_bus enter [ 3.289555] Rio_debug cdns_pci_map_bus enter [ 3.293821] Rio_debug cdns_pci_map_bus enter [ 3.298085] Rio_debug cdns_pci_map_bus enter [ 3.302351] Rio_debug cdns_pci_map_bus enter [ 3.306616] Rio_debug cdns_pci_map_bus enter [ 3.310881] Rio_debug cdns_pci_map_bus enter [ 3.315146] Rio_debug cdns_pci_map_bus enter [ 3.319413] Rio_debug cdns_pci_map_bus enter [ 3.323678] Rio_debug cdns_pci_map_bus enter [ 3.327943] Rio_debug cdns_pci_map_bus enter [ 3.332210] Rio_debug cdns_pci_map_bus enter [ 3.336482] Rio_debug cdns_pci_map_bus enter [ 3.340753] Rio_debug cdns_pci_map_bus enter [ 3.345020] Rio_debug cdns_pci_map_bus enter [ 3.349286] Rio_debug cdns_pci_map_bus enter [ 3.353552] Rio_debug cdns_pci_map_bus enter [ 3.357820] pci 0000:01:00.0: PME# supported from D0 D3hot [ 3.363302] Rio_debug cdns_pci_map_bus enter [ 3.367568] Rio_debug cdns_pci_map_bus enter [ 3.371835] Rio_debug cdns_pci_map_bus enter [ 3.376100] Rio_debug cdns_pci_map_bus enter [ 3.380366] Rio_debug cdns_pci_map_bus enter [ 3.384631] Rio_debug cdns_pci_map_bus enter [ 3.388900] Rio_debug cdns_pci_map_bus enter [ 3.393166] Rio_debug cdns_pci_map_bus enter [ 3.397432] Rio_debug cdns_pci_map_bus enter [ 3.401700] Rio_debug cdns_pci_map_bus enter [ 3.405967] Rio_debug cdns_pci_map_bus enter [ 3.410233] Rio_debug cdns_pci_map_bus enter [ 3.414499] Rio_debug cdns_pci_map_bus enter [ 3.418767] Rio_debug cdns_pci_map_bus enter [ 3.423034] Rio_debug cdns_pci_map_bus enter [ 3.427298] Rio_debug cdns_pci_map_bus enter [ 3.431565] Rio_debug cdns_pci_map_bus enter [ 3.435830] Rio_debug cdns_pci_map_bus enter [ 3.440097] Rio_debug cdns_pci_map_bus enter [ 3.444363] Rio_debug cdns_pci_map_bus enter [ 3.448628] Rio_debug cdns_pci_map_bus enter [ 3.452892] Rio_debug cdns_pci_map_bus enter [ 3.457158] Rio_debug cdns_pci_map_bus enter [ 3.461427] Rio_debug cdns_pci_map_bus enter [ 3.465693] Rio_debug cdns_pci_map_bus enter [ 3.470098] Rio_debug cdns_pci_map_bus enter [ 3.474366] Rio_debug cdns_pci_map_bus enter [ 3.478635] Rio_debug cdns_pci_map_bus enter [ 3.482902] Rio_debug cdns_pci_map_bus enter [ 3.487168] Rio_debug cdns_pci_map_bus enter [ 3.491434] Rio_debug cdns_pci_map_bus enter [ 3.495802] Rio_debug cdns_pci_map_bus enter [ 3.500072] Rio_debug cdns_pci_map_bus enter [ 3.504337] Rio_debug cdns_pci_map_bus enter [ 3.508604] Rio_debug cdns_pci_map_bus enter [ 3.512869] Rio_debug cdns_pci_map_bus enter [ 3.517132] Rio_debug cdns_pci_map_bus enter [ 3.521401] Rio_debug cdns_pci_map_bus enter [ 3.525669] Rio_debug cdns_pci_map_bus enter [ 3.529929] Rio_debug cdns_pci_map_bus enter [ 3.534195] Rio_debug cdns_pci_map_bus enter [ 3.538453] Rio_debug cdns_pci_map_bus enter [ 3.542716] Rio_debug cdns_pci_map_bus enter [ 3.546981] Rio_debug cdns_pci_map_bus enter [ 3.551245] Rio_debug cdns_pci_map_bus enter [ 3.555507] Rio_debug cdns_pci_map_bus enter [ 3.559511] Rio_debug: j721e_pcie_link_irq_handler --entered [ 3.565404] LINK DOWN! [ 4.688666] Rio_debug cdns_pci_map_bus enter [ 4.692944] Rio_debug cdns_pci_map_bus enter [ 4.697211] Rio_debug cdns_pci_map_bus enter [ 4.701476] Rio_debug cdns_pci_map_bus enter [ 4.705745] Rio_debug cdns_pci_map_bus enter [ 4.710009] Rio_debug cdns_pci_map_bus enter [ 4.714276] Rio_debug cdns_pci_map_bus enter [ 4.718565] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01 [ 4.725179] Rio_debug cdns_pci_map_bus enter [ 4.729444] Rio_debug cdns_pci_map_bus enter [ 4.733738] pci 0000:00:00.0: BAR 0: no space for [mem size 0x1000000000 64bit pref] [ 4.741477] pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x1000000000 64bit pref] [ 4.749568] pci 0000:00:00.0: BAR 14: assigned [mem 0x68100000-0x681fffff] [ 4.756443] pci 0000:01:00.0: BAR 0: assigned [mem 0x68100000-0x68103fff] [ 4.763226] Rio_debug cdns_pci_map_bus enter [ 4.767492] Rio_debug cdns_pci_map_bus enter [ 4.771760] pci 0000:00:00.0: PCI bridge to [bus 01] [ 4.776721] Rio_debug cdns_pci_map_bus enter [ 4.780986] Rio_debug cdns_pci_map_bus enter [ 4.785250] Rio_debug cdns_pci_map_bus enter [ 4.789515] pci 0000:00:00.0: bridge window [mem 0x68100000-0x681fffff] [ 4.796299] Rio_debug cdns_pci_map_bus enter [ 4.800562] Rio_debug cdns_pci_map_bus enter [ 4.804825] Rio_debug cdns_pci_map_bus enter [ 4.809091] Rio_debug cdns_pci_map_bus enter [ 4.813356] Rio_debug cdns_pci_map_bus enter [ 4.817620] Rio_debug cdns_pci_map_bus enter [ 4.822039] Rio_debug cdns_pci_map_bus enter [ 4.826309] Rio_debug cdns_pci_map_bus enter [ 4.830662] Rio_debug j721e_pcie_intx_map enter [ 4.835194] Rio_debug cdns_pci_map_bus enter [ 4.839462] Rio_debug cdns_pci_map_bus enter [ 4.843727] Rio_debug cdns_pci_map_bus enter [ 4.847992] pcieport 0000:00:00.0: enabling device (0000 -> 0002) [ 4.854081] Rio_debug cdns_pci_map_bus enter [ 4.858347] Rio_debug cdns_pci_map_bus enter [ 4.862610] Rio_debug cdns_pci_map_bus enter [ 4.866877] Rio_debug cdns_pci_map_bus enter [ 4.871134] Rio_debug cdns_pci_map_bus enter [ 4.875402] Rio_debug cdns_pci_map_bus enter [ 4.879667] Rio_debug cdns_pci_map_bus enter [ 4.883932] Rio_debug cdns_pci_map_bus enter [ 4.888196] Rio_debug cdns_pci_map_bus enter [ 4.892458] Rio_debug cdns_pci_map_bus enter [ 4.896724] Rio_debug cdns_pci_map_bus enter [ 4.900989] Rio_debug cdns_pci_map_bus enter [ 4.905252] Rio_debug cdns_pci_map_bus enter [ 4.909516] Rio_debug cdns_pci_map_bus enter [ 4.913790] Rio_debug cdns_pci_map_bus enter [ 4.918056] Rio_debug cdns_pci_map_bus enter [ 4.922319] Rio_debug cdns_pci_map_bus enter [ 4.926583] Rio_debug cdns_pci_map_bus enter [ 4.930847] Rio_debug cdns_pci_map_bus enter [ 4.935114] Rio_debug cdns_pci_map_bus enter [ 4.939379] Rio_debug cdns_pci_map_bus enter [ 4.943643] Rio_debug cdns_pci_map_bus enter [ 4.947908] Rio_debug cdns_pci_map_bus enter [ 4.952173] Rio_debug cdns_pci_map_bus enter [ 4.956437] Rio_debug cdns_pci_map_bus enter [ 4.960702] Rio_debug cdns_pci_map_bus enter [ 4.964966] Rio_debug cdns_pci_map_bus enter [ 4.969238] Rio_debug cdns_pci_map_bus enter [ 4.973607] Rio_debug cdns_pci_map_bus enter [ 4.977906] Rio_debug cdns_pci_map_bus enter [ 4.982173] Rio_debug cdns_pci_map_bus enter [ 4.986439] Rio_debug cdns_pci_map_bus enter [ 4.990703] Rio_debug cdns_pci_map_bus enter [ 4.994971] Rio_debug cdns_pci_map_bus enter [ 4.999250] Rio_debug cdns_pci_map_bus enter [ 5.003520] Rio_debug cdns_pci_map_bus enter [ 5.007783] Rio_debug cdns_pci_map_bus enter [ 5.012046] Rio_debug cdns_pci_map_bus enter [ 5.016313] Rio_debug cdns_pci_map_bus enter [ 5.020577] Rio_debug cdns_pci_map_bus enter [ 5.024962] Rio_debug cdns_pci_map_bus enter [ 5.029221] Rio_debug cdns_pci_map_bus enter [ 5.033486] Rio_debug cdns_pci_map_bus enter [ 5.037750] Rio_debug cdns_pci_map_bus enter [ 5.042025] Rio_debug cdns_pci_map_bus enter [ 5.046344] pcieport 0000:00:00.0: PME: Signaling with IRQ 502 [ 5.052177] Rio_debug cdns_pci_map_bus enter [ 5.056433] Rio_debug cdns_pci_map_bus enter [ 5.061088] Rio_debug cdns_pci_map_bus enter [ 5.065391] Rio_debug cdns_pci_map_bus enter [ 5.069658] Rio_debug cdns_pci_map_bus enter [ 5.073915] Rio_debug cdns_pci_map_bus enter [ 5.078178] Rio_debug cdns_pci_map_bus enter [ 5.082442] Rio_debug cdns_pci_map_bus enter [ 5.086705] Rio_debug cdns_pci_map_bus enter [ 5.090969] Rio_debug cdns_pci_map_bus enter [ 5.095232] Rio_debug cdns_pci_map_bus enter [ 5.099496] Rio_debug cdns_pci_map_bus enter [ 5.103762] Rio_debug cdns_pci_map_bus enter [ 5.108025] Rio_debug cdns_pci_map_bus enter [ 5.112291] Rio_debug cdns_pci_map_bus enter [ 5.116555] Rio_debug cdns_pci_map_bus enter [ 5.120821] pcieport 0000:00:00.0: AER: enabled with IRQ 502 [ 5.126616] Rio_debug cdns_pci_map_bus enter [ 5.130884] Rio_debug cdns_pci_map_bus enter [ 5.135149] Rio_debug cdns_pci_map_bus enter [ 5.139412] Rio_debug cdns_pci_map_bus enter [ 5.143674] Rio_debug cdns_pci_map_bus enter [ 5.147940] Rio_debug cdns_pci_map_bus enter [ 5.152205] Rio_debug cdns_pci_map_bus enter [ 5.156468] Rio_debug cdns_pci_map_bus enter [ 5.160733] Rio_debug cdns_pci_map_bus enter [ 5.164997] Rio_debug cdns_pci_map_bus enter [ 5.169261] Rio_debug cdns_pci_map_bus enter [ 5.173524] Rio_debug cdns_pci_map_bus enter [ 5.177786] Rio_debug cdns_pci_map_bus enter [ 5.182050] Rio_debug cdns_pci_map_bus enter [ 5.186319] Rio_debug cdns_pci_map_bus enter [ 5.190584] Rio_debug cdns_pci_map_bus enter [ 5.194849] Rio_debug cdns_pci_map_bus enter [ 5.199114] Rio_debug cdns_pci_map_bus enter [ 5.203378] Rio_debug cdns_pci_map_bus enter [ 5.207642] Rio_debug cdns_pci_map_bus enter [ 5.211905] Rio_debug cdns_pci_map_bus enter [ 5.216169] Rio_debug cdns_pci_map_bus enter [ 5.220434] Rio_debug cdns_pci_map_bus enter [ 5.224700] Rio_debug cdns_pci_map_bus enter [ 5.228964] Rio_debug cdns_pci_map_bus enter [ 5.233228] Rio_debug cdns_pci_map_bus enter [ 5.237490] Rio_debug cdns_pci_map_bus enter [ 5.241753] Rio_debug cdns_pci_map_bus enter [ 5.246020] Rio_debug cdns_pci_map_bus enter [ 5.250284] Rio_debug cdns_pci_map_bus enter [ 5.254547] Rio_debug cdns_pci_map_bus enter [ 5.258809] Rio_debug cdns_pci_map_bus enter [ 5.263072] Rio_debug cdns_pci_map_bus enter [ 5.267333] Rio_debug cdns_pci_map_bus enter [ 5.271597] Rio_debug cdns_pci_map_bus enter [ 5.275860] Rio_debug cdns_pci_map_bus enter [ 5.280122] Rio_debug cdns_pci_map_bus enter [ 5.284384] Rio_debug cdns_pci_map_bus enter [ 5.288651] Rio_debug cdns_pci_map_bus enter [ 5.292916] Rio_debug cdns_pci_map_bus enter [ 5.297216] Rio_debug cdns_pci_map_bus enter [ 5.301503] Rio_debug cdns_pci_map_bus enter [ 5.305772] Rio_debug cdns_pci_map_bus enter [ 5.310037] Rio_debug cdns_pci_map_bus enter [ 5.314300] Rio_debug cdns_pci_map_bus enter [ 5.318563] Rio_debug cdns_pci_map_bus enter [ 5.322827] Rio_debug cdns_pci_map_bus enter [ 5.327091] Rio_debug cdns_pci_map_bus enter [ 5.331355] Rio_debug cdns_pci_map_bus enter [ 5.335620] Rio_debug cdns_pci_map_bus enter [ 5.339885] Rio_debug cdns_pci_map_bus enter [ 5.344148] Rio_debug cdns_pci_map_bus enter [ 5.348410] Rio_debug cdns_pci_map_bus enter [ 5.352675] Rio_debug cdns_pci_map_bus enter [ 5.356938] Rio_debug cdns_pci_map_bus enter [ 5.361202] Rio_debug cdns_pci_map_bus enter [ 5.365470] Rio_debug cdns_pci_map_bus enter [ 5.369733] Rio_debug cdns_pci_map_bus enter [ 5.374011] Rio_debug cdns_pci_map_bus enter [ 5.378289] Rio_debug cdns_pci_map_bus enter [ 5.382553] Rio_debug cdns_pci_map_bus enter [ 5.386816] Rio_debug cdns_pci_map_bus enter [ 5.391079] Rio_debug cdns_pci_map_bus enter [ 5.395341] Rio_debug cdns_pci_map_bus enter [ 5.399606] Rio_debug cdns_pci_map_bus enter [ 5.403869] Rio_debug cdns_pci_map_bus enter [ 5.408133] Rio_debug cdns_pci_map_bus enter [ 5.412395] Rio_debug cdns_pci_map_bus enter [ 5.416660] Rio_debug cdns_pci_map_bus enter [ 5.420923] Rio_debug cdns_pci_map_bus enter [ 5.432415] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present! [ 5.440057] mmc1: CQHCI version 5.10 [ 5.450756] ALSA device list: [ 5.453762] No soundcards found. [ 5.484361] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit [ 5.492149] Waiting for root device PARTUUID=56bb290c-02... [ 5.545933] mmc1: new ultra high speed SDR104 SDHC card at address aaaa [ 5.553520] mmcblk1: mmc1:aaaa SE32G 29.7 GiB [ 5.561751] mmcblk1: p1 p2 [ 5.608365] EXT4-fs (mmcblk1p2): recovery complete [ 5.613901] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none. [ 5.622538] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 5.633433] devtmpfs: mounted [ 5.637858] Freeing unused kernel memory: 2112K [ 5.642507] Run /sbin/init as init process [ 5.725892] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none. Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting system message bus: [ 6.816667] random: crng init done done Starting iptables: OK Starting network: OK Welcome to Advantech device server EKI series adv-eki login: