Other Parts Discussed in Thread: SYSBIOS, TMS570LS20216
Hello,
I know there's a bug in the code that does not update the ROV view correctly (Bug id: SDOCM00083550). It seems that isn't the only problem. The Hwi_setPriority doesn't seem to set the priority specified correctly in the hardware. In fact my interrupt do not comes anymore when I change the priority.
For instance:
Hwi_setPriority( 3, TMS570::DrvVim::VIM_HET_HIGH + 1 ); //Lower the priority of BIOS tick (a timer) compare to another isr.
Here I'm trying to lower the priority of my timer (clock tick). If I call this function, the timer doesn't work anymore. Same thing for other interrupt in the TMS570. My VIM_HET_HIGH doesn't work anymore if I'm trying to raise to 3.
Simon
My setup:
sysbios 6.31.4.27, xdc 3.20.8.88, ccs5.1