Other Parts Discussed in Thread: UNIFLASH
Hi, Experts
I want to check if HS board keywriter programming sequence is feasible.
Back ground is customer use OSPI Norflash as boot media to mass production.
Here is the sequence step by step, please help to double check:
Signed tiboot.bin and other boot files
Use uniflash to store the boot image to Nor flash.
Boot mode on Board is
Connect PC host to Board through DFU.
Power on, Rom fistly use ospi boot mode to boot, failed because Key have't been wrote to board.
Then Rom jump to backup boot mode, which is DFU boot mode. Keywriter will be used as SBL and boot, key is flashed into ROM.
Power off, power on. Now Rom can succeed to boot use Nor flash boot image.
Please help to check if it is feasible of whole process? Thanks.
Regards
Zekun