Part Number: SK-AM69
Other Parts Discussed in Thread: TMDSEMU560V2STM-U, AM69
Hi TI,
I'm using a SK-AM69 and a brand new usb560v2 debugger connected to J15 20-pin CTI header for the first time.
I've installed Bh560v2Config v 1.0.0.14 and it's recognizes the debugger. But if I run the tests I am receiving the following error:
Blackhawk Configuration Utility Tests
CMD: dbgjtag -X emulator,driver=bh560v2u,ioport=0 -S integrity -Y reset -S pathlength
Loaded FPGA Image: C:\ti\ccs1260\ccs\ccs_base\common\uscif\dtc_top.jbc
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-180' (0xffffff4c).
The title is 'SC_ERR_CTL_NO_TRG_POWER'.
The explanation is:
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
RES: dbgjtag -X emulator,driver=bh560v2u,ioport=0 -S integrity -Y reset -S pathlength
RES: Fail
Via CCSv12.7 I'm receiving this error:
CCS Test Connection
[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\549KRA~1\AppData\Local\TEXASI~1\
CCS\ccs1260\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
Loaded FPGA Image: C:\ti\ccs1260\ccs\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Mar 13 2024'.
The library build time was '12:55:46'.
The library package version is '12.7.0.00105'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-180' (0xffffff4c).
The title is 'SC_ERR_CTL_NO_TRG_POWER'.
The explanation is:
The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target.
[End: Blackhawk XDS560v2-USB System Trace Emulator_0]
Both mention the power loss of the targets device, but checking the targets voltage on pin 5 of J15, I measure 3.3V.

The onboard debugger XDS110 is working fine though.
Does anyone has seen this before?
To me it seems that the USB560v2 debugger is broken.
Best,
Kim