This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5535 eZdsp error programming SPI onboard RAM

 

Hello,

I am getting this error (see below please), when I try to download an .img file to the 8Mb SPI ram.

Same file is correctly bootloaded and run from the SD card.

I have tried at 100Mhz and preseting the PLL to 12MHz..

Help is welcomed.

 

Choose the device...
1<filepath> - NOR Flash
2<filepath> - NAND Flash
3<filepath> - SPI
4<filepath> - IIC EEPROM
5<filepath> - MMC
6<filepath> - SD
3C:\eZdspIMAGES\bootimg1.bin
SPI...
Writing data to device...
Opening C:\eZdspIMAGES\bootimg1.bin...
Input file opened
WRITE ERROR! at 0x00000000
Wrote 0x09aa Read 0x0000

Thanks,

Maximiliano