This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

serious problems



hi !

SDK = ezsdk502(latest)  

base board = ti8168

using FBDev sample application to test HDCOMP and SDVENC output.

frist > my steps

|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_| 
              |___|                    |___|           

Arago Project http://arago-project.org dm816x-evm ttyO2

Arago 2011.05 dm816x-evm ttyO2

dm816x-evm login: root
root@dm816x-evm:~# /etc/init.d/matrix-gui-e stop
Stopping Matrix GUI application.
root@dm816x-evm:~# cd /home/video-test/
root@dm816x-evm:/home/video-test# ./saFbdevDisplay

Fix Screen Info:
----------------
Line Length - 7680
Physical Address = 8ce00000
Buffer Length = 25165824

Var Screen Info:
----------------
Xres - 1920
Yres - 1080
Xres Virtual - 1920
Yres Virtual - 3240
Bits Per Pixel - 32
Pixel Clk - 6734
Rotation - 0
root@dm816x-evm:/home/video-test#

note : it is ok .output from on-chip-hdmi is ok

in order to test HD-DAC (hdcomp)

root@dm816x-evm:/home/video-test# ./saFbdevDisplay-hdcomp

note : changed
static char display_dev_name[30] = {"/dev/fb0"};

to
static char display_dev_name[30] = {"/dev/fb1"};

but it is not ok ,"NO SINGNAL INPUT" is displayed on the screen connected to ti8168 through HD-DAC interface

 

in order to test SD-DAC (composite&s-video)

root@dm816x-evm:/home/video-test# ./saFbdevDisplay-sdcomp

note : changed
static char display_dev_name[30] = {"/dev/fb0"};

to
static char display_dev_name[30] = {"/dev/fb2"};

but it is not ok ,"NO SINGNAL INPUT" is displayed on the screen connected to ti8168 through SD-DAC interface

i am sure all the devices are ok

why why why why????????????????????????????????????????

second > try

1.power off  base board then power on

2. run the omtb demo

                         root@dm816x-evm:/usr/share/ti/ti-omtb# ./omtb_dm816xbm_a8host.xv5T decode_scale_display.oms 

                        note : i changed  the below in oder to watch video from HD-DAC(HDCOMP) interface

                         omx setp 0 vfdc OMX_TI_IndexParamVFDCDriverInstId nDrvInstID 1

 

                         omx setp 0 dc OMX_TI_IndexParamVFDCDriverInstId nDrvInstID 1

                          now  it is ok

3. in order stop the demo i reboot the board (CTRL + C can not stop it )

4.now how is amazing   i operate all  the frist steps  all are ok 

                           ON-CHIP-HDMI     HD-DAC         SD-DAC    all worked

5. then i power off then power on the board

                           HD-DAC         SD-DAC   can not  work  no picture/video output

why why why why why ???????????????????????????????????????

third > what i want to do is test HD-DAC  SD-DAC  interface