This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to install TSC2046EVM software

My PC failed to enumerate the USB PC driver for TSC2046EVM-PDK after I attached the USB cable. The USB ACTIVE LED(D2) is not lit up. I followed the user guide to install the software from CD-ROM and then installed the NI-VISA 3.1. The hardware wizard always shows the unknown device after I attached the USB cable. I am using default setting for all the jumpers. My PC is Windows XP SP2 system.  I've checked that the hardware wizard has detected the USB device with VID_FFFF as vendor ID, and that is probably why the system failed to find a device driver.

 

Anyone can help me to install the USB driver?

 

Thanks,

Eric

  • Eric,

    To make sure the D2 is ON, please check --

    (1) The TSC2046EVM board is on the up/middle position of the USB-MODEVM board, connecting with J11, J12 and J13 of the USB-MODEVM.

    (2) The SW2 on the USB-MODEVM board is switched in such a way that at least one of SW2-1, SW2-2, and SW2-3 (i.e. A0, A1, and A2)  is OFF.

    After double checked the above, tell me what you got now!

    Regards,
    Wendy F.