Are there plans to fix the limitation that you cannot have graphics if you are using C6run?
I refer to the software developer's guide in EZSDK 5.02.02.60:
"The C6Run samples cannot be run without first bringing down the graphics plane"
Also it says: "The C6Accel apps should not be run out with graphics. Please execute the following steps to teardown the graphics plane and ensure that no firmware is running."
Why does it say this when the Signal Analyzer demo clearly uses graphics and C6accel?
I am confused.
Thanks,
Ralph