This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reset Timing on the OMAP-L138

Other Parts Discussed in Thread: OMAP-L138

I have a customer who is working with the OMAP-L138 and the LogicPD L138 Dev. Board.

"I've been scouring the L138 documentation for the Reset pin's rise/fall time requirement.  Currently, just like the the SOM-M1 from LogicPD, we use a 4.7k pullup and a 100nF cap tied directly to the pin.  This yields a fairly slow ramp up after a reset occurs - approximately 1mS.  Is this a problem given the errata 2.0.20?  Can you point me to the electrical specification?"

Help is appreciated!