This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: Is it possible to transfer data via USB-C?

Part Number: SK-AM62A-LP

I'm planning on buying the SK-AM62A-LP module for a project and would like to know if it's possible to supply the power with usb-c connected to a computer while also transferring data.

Thanks in advance for your help!

  • Hi Joaquin,

    The SK EVM has two USB type-C connectors. One of them is routed to the AM62A USB0 module, this USB-C port is also routed to the PMIC devices. So you can power the SK EVM and also transfer data using this USB-C port, However, the USB2.0 Specification defines the maximum draw current from a USB2.0 port is 500mA, this may not be enough to power the SK EVM depending on your use cases.