Hi,
I connected to USB-Camera on USB-A port in SK-TDA4VM but when the device connected to the kit isn't recognized.
I acquired these kind of log code which I don't know about when connecting the camera.
Would you please let me know if the log specifies something unusual which part is wrong?
I hope I could connect normally.
If not, I hope I can exchange good one.
Error case
|
### hotplug… NGGGGGGGG [ 58.607191] usb 1-1.2: new full-speed USB device number 4 using xhci-hcd [ 58.723165] usb 1-1.2: not running at top speed; connect to a high speed hub [ 58.833856] usb 1-1.2: Found UVC 1.10 device ABKO APC925 QHD WEBCAM (1bcf:2cb4) [ 58.898444] usb 1-1.2: Failed to query (GET_INFO) UVC control 9 on unit 1: -32 (exp. 1). [ 58.917288] usb 1-1.2: UVC non compliance - GET_DEF(PROBE) not supported. Enabling workaround. [ 58.930328] uvcvideo 1-1.2:1.1: Failed to query (129) UVC probe control : 26 (exp. 34). [ 58.938327] uvcvideo 1-1.2:1.1: Failed to initialize the device (-5). [ 58.944898] usbcore: registered new interface driver uvcvideo |
Normal Case
|
[ 30.842210] usb 1-1.2: Found UVC 1.00 device ABKO APC925 QHD WEBCAM (1bcf:2cb4) [ 30.929893] input: ABKO APC925 QHD WEBCAM: ABKO AP as /devices/platform/bus@100000/4114000.cdns-usb/6400000.usb/xhci-hcd.6.auto/usb1/1-1/1-1.2/1-1.2:1.0/input/input4 [ 30.944828] usbcore: registered new interface driver uvcvideo [ 31.149353] usb 1-1.2: 3:1: cannot get freq at ep 0x86 [ 31.348665] usb 1-1.2: 3:2: cannot get freq at ep 0x86 [ 31.547969] usb 1-1.2: 3:3: cannot get freq at ep 0x86 [ 32.560591] usb 1-1.2: Warning! Unlikely big volume range (=4096), cval->res is probably wrong. [ 32.569287] usb 1-1.2: [7] FU [Mic Capture Volume] ch = 1, val = 0/4096/1 [ 32.576343] usbcore: registered new interface driver snd-usb-audio |