Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM
Hi, I have several question about commands in SK-TDA4VM.
(1)
Link LED of ethernet port is OFF on at SK-TDA4VM while I could ping gateway after setting ip/gateway at bootmode..
I seems it has not been linked up.
Is there anything else to set up for link up?
|
setenv ipaddr=10.11.72.23 (available ip) root@tda4vm-sk:/opt/edgeai-gst-apps# ping 10.11.72.254 |
(2)
|
=> usb dev
no usb devices available
|
Which test is the usb test in the boot mode ?
|
usb test [dev] [port] [mode] - set USB 2.0 test mode
(specify port 0 to indicate the device's upstream port)
Available modes: J, K, S[E0_NAK], P[acket], F[orce_Enable]
|
(4)
Is there any bash shell commands list performed in SK-TDA4VM which can test the board condition ?
We just want to check the SK-TDA4VM is OK with shell command first.
If TI performed any boot command for checking out the EV board, would you share the list if it is OK?
Is there any command for diag test such as emmc memory/ DDR4/ CPU load/ ?
(6)
How can we monitor TDA4VM chip temperature by command at SK-TDA4VM ?
Do we need to set watchdog disable when developing via SK-TDA4VM image?
How can we disable watchdog then?