Hi,
- I'm running the PA_emacExample_exampleProject example from the MCDSK 2_00_00)14, first time everything works fine, running it the second time after restarting or after CPU reset it fails at "Setup_PASS ()" , only re-power the board helps -
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Tx setup successfully done
[C66xx_0] Rx setup successfully done
[C66xx_0] Timeout waiting for reply from PA to Pa_addMac command
[C66xx_0] PASS setup failed
Any reason for this?
- In the case that the buffers are in teh DDR3 than I think that there is a need to add to the function "Convert_CoreLocal2GlobalAddr" a test if the address is a global one,
Thanks,
HR