Part Number: AM623
Other Parts Discussed in Thread: AM625
Hi experts
The customer's project using AM6231 is ready for small batch production. However, there is a problem that is currently stuck and cannot continue, and we hope that it will be supported.
The symptoms are as follows:
1.EtherCAT master has packet loss (1 ms send once, Codesys or system driver statistics within half an hour of data retrieval is about 30 packets less than data sent)
2.Packet loss is also can be reproduced using TI's am625 EVM and SDK;
3.The transmission frequency becomes low (more than 3ms sent once) packet loss is relieved; the NIC driver statistics no error;
4.The customer is convinced that it is not the problem of other sites connected to the network port, because they tried the PLC of other companies in the same environment without losing the packet.
I suspect it is related to the configuration of the Ethernet port or the Ethernet driver