This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: I wanted to flash custom images into the images of the evk,which have the following components

Part Number: SK-AM62B-P1
Other Parts Discussed in Thread: UNIFLASH

I wanted to flash custom images into the images of the evk,which have the following components:

  • A boot patition
    • tiboot3.bin
    • tispl.bin
    • u-boot.img
    • uboot.env
  • A ext4 partition in the user data area containing
    • Linux Kernel image
    • Linux DTB
    • Linux file system

      suraj@suraj-HP-Laptop-15s-fr2xxx:/opt/ti-processor-sdk-linux-am62xx-evm-09.02.01.09/bin/uart_uniflash$ sudo python3 uart_uniflash.py -p /dev/ttyUSB0 --cfg=/home/suraj/Downloads/uart_flash.cfg
      
      Parsing config file ...
      Parsing config file ... SUCCESS. Found 7 command(s) !!!
      
      Executing command 1 of 7 ...
      Found flash writer ... sending /opt/ti-processor-sdk-linux-am62xx-evm-09.02.01.09/bin/uart_uniflash/bin/am62xx-evm/sbl_uart_uniflash_stage1.release.hs_fs.tiimage
      Sent flashwriter /opt/ti-processor-sdk-linux-am62xx-evm-09.02.01.09/bin/uart_uniflash/bin/am62xx-evm/sbl_uart_uniflash_stage1.release.hs_fs.tiimage of size 246687 bytes in 23.84s.                         
      
      Executing command 2 of 7 ...
      Command arguments : --file=/opt/ti-processor-sdk-linux-am62xx-evm-09.02.01.09/bin/uart_uniflash/bin/am62xx-evm/sbl_uart_uniflash_stage2.release.appimage.hs_fs --operation=flash --flash-offset=0x0
      Sent /opt/ti-processor-sdk-linux-am62xx-evm-09.02.01.09/bin/uart_uniflash/bin/am62xx-evm/sbl_uart_uniflash_stage2.release.appimage.hs_fs of size 122931 bytes in 15.11s.                                    
      [STATUS] SUCCESS !!!
      
      Executing command 3 of 7 ...
      Command arguments : --file=/home/suraj/Downloads/tiboot3-am62x-hs-fs-evm.bin --operation=flash --flash-offset=0x0
      Sent /home/suraj/Downloads/tiboot3-am62x-hs-fs-evm.bin of size 295438 bytes in 31.51s.                                                                                                                      
      [STATUS] SUCCESS !!!
      
      Executing command 4 of 7 ...
      Command arguments : --file=/home/suraj/Downloads/tispl.bin-am62xx-evm --operation=flash --flash-offset=0x80000
      Sent /home/suraj/Downloads/tispl.bin-am62xx-evm of size 1178343 bytes in 116.58s.                                                                                                                           
      [STATUS] SUCCESS !!!
      
      Executing command 5 of 7 ...
      Command arguments : --file=/home/suraj/Downloads/u-boot-am62xx-evm.img --operation=flash --flash-offset=0x280000
      Sent /home/suraj/Downloads/u-boot-am62xx-evm.img of size 984939 bytes in 95.35s.                                                                                                                            
      [STATUS] SUCCESS !!!
      
      Executing command 6 of 7 ...
      Command arguments : --file=/home/suraj/Downloads/agl-demo-platform-am62xx-evm-20240416145915.rootfs/boot/Image --operation=flash --flash-offset=0x83000000
      Sent /home/suraj/Downloads/agl-demo-platform-am62xx-evm-20240416145915.rootfs/boot/Image of size 24447488 bytes in 2366.150000000001s.                                                                      
      [STATUS] ERROR: Flashing failed !!!
      
      Executing command 7 of 7 ...
      Command arguments : --file=/home/suraj/Downloads/agl-demo-platform-am62xx-evm-20240416145915.rootfs/boot/dtb/ti/k3-am625-sk.dtb --operation=flash --flash-offset=0x83080000
      Sent /home/suraj/Downloads/agl-demo-platform-am62xx-evm-20240416145915.rootfs/boot/dtb/ti/k3-am625-sk.dtb of size 61983 bytes in 8.86s.                                                                     
      [STATUS] ERROR: Flashing failed !!!
      
      All commands from config file are executed !!!


      This is the output to flash all the images using uart uniflash script.


      U-Boot 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
      
      SoC:   AM62X SR1.0 HS-FS
      Model: Texas Instruments AM625 SK
      EEPROM not available at 80, trying to read at 81
      Board: AM62B-SKEVM-P1 rev A
      DRAM:  2 GiB
      Core:  72 devices, 32 uclasses, devicetree: separate
      MMC:   mmc@fa10000: 0, mmc@fa00000: 1
      Loading Environment from nowhere... OK
      In:    serial
      Out:   serial
      Err:   serial
      Net:   eth0: ethernet@8000000port@1
      Hit any key to stop autoboot:  0 
      => mmc dev 0 0
      switch to partitions #0, OK
      mmc0(part 0) is current device
      => mmc part
      
      Partition Map for MMC device 0  --   Partition Type: DOS
      
      Part    Start Sector    Num Sectors     UUID            Type
        1     2048            32768           0d0c5ad5-01     0e Boot
        2     34816           31045632        0d0c5ad5-02     83
      => ls mmc 0:2
      => ls mmc 0:2 /boot
      => ls mmc 0:2 /boot/dtb/ti
      => mmc part
      
      Partition Map for MMC device 0  --   Partition Type: DOS
      
      Part    Start Sector    Num Sectors     UUID            Type
        1     2048            32768           0d0c5ad5-01     0e Boot
        2     34816           31045632        0d0c5ad5-02     83


      This is the output after flash.


      This are the logs , i have tried many times to flash all the images using uart uniflash script, now u-boot images are flashing but kernel and dtb images both are not flashing in logs u can see last two images are showing failed to flash please give any solution asap.