Other Parts Discussed in Thread: SYSBIOS
Hello
I have a question. I try to run Ethernet/IP adapter example on Am335x icev2.1 board. I am not able to ping this board from my PC.
1. when I use these
PRU-ICSS-EthernetIP_Adapter-01.00.03.04
pdk_am335x_1_0_12
SYS_BIOS_VERSION=6.73.00.12
XDC_TOOLS_VERSION=3.50.07.20_core
NDK_VERSION=3.40.01.01
EDMA_VERSION=2.12.05.30
to create project . To ping this board is ok!
2. when I use these
PRU-ICSS-EthernetIP_Adapter_01.00.04.11
pdk_am335x_1_0_17
SYS_BIOS_VERSION=6.76.03.01
XDC_TOOLS_VERSION=3.55.02.22_core
NDK_VERSION=3.61.01.01
EDMA_VERSION=2.12.05.30
to create project . To ping this board is bad! (I change the same IP address.)
I can get the massage on my screen:
Start IO
MAC : 2c:6b:7d:49:f6:36
ACD Bit Enabled in Flash. Starting the Application in ACD Mode
IP Address will be taken once Link is up
IP Address obtained from Flash
IP Address Assigned: 192.168.1.3
my board is AM335x ICE rev 2.1A. what's happen?