Other Parts Discussed in Thread: WL1271
Hi,
I am looking for EDMA3 example project for the M3 on the DM8148 device. Do we have an example?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: WL1271
Hi,
I am looking for EDMA3 example project for the M3 on the DM8148 device. Do we have an example?
Hi Prashanth,
Basically what I found out is that the latest release 02.11.02.04 of the edma3 LLD for BIOS-6 contains m3 versions of :
- LLD driver under edma3_lld_02_11_02_04\packages\ti\sdo\edma3\drv\lib\m3
- RM driver under edma3_lld_02_11_02_04\packages\ti\sdo\edma3\rm\lib\ti816x-evm\m3
I believe both libraries should work fine on dm814x. Although there is no ti814x equivalent for the file sample_ti816x_m3vpss_cfg.c and sample_ti816x_m3vpss_int_reg.c under edma3_lld_02_11_02_04\packages\ti\sdo\edma3\rm\sample\src\platforms, I have been told they should be applicable to ti814x as well because the EDMA addresses and interrupts are the same between the two platforms.
regards,
Victor
Note that in release 02.11.02.04 the CCS4.x, the sample project located in edma3_lld_02_11_02_04\examples\edma3_driver\evmTI816x_ARM\sample_app is supposed to build the executable for the M3 but the compiler target was wrongly set to Cortex A8, not M3.
The makefile doesn't have this issue though.
Also note that for dm814x, I could use the dm816x's edma configuration file edma3_lld_02_11_02_04\packages\ti\sdo\edma3\rm\sample\src\platforms\sample_ti816x_m3vpss_cfg.c and it worked fine.
Hello
Do you know what EDMA3 channel that I need dispatch to MMC3 in DM8148?
Our projectj use MMC3 to connect WL1271 SDIO interface, but , when start DMA transfer ,there is a dataabort, I analyse it is because that I use wrong DMA channel, but I don't know what channel I should use. Could you help me, thank!
Hello Do you know what EDMA3 channel that I need dispatch to MMC3 in DM8148? Our projectj use MMC3 to connect WL1271 SDIO interface, but , when start DMA transfer ,there is a dataabort, I analyse it is because that I use wrong DMA channel, but I don't know what channel I should use. Could you help me, thank!