This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: Compatible replacement devices

Guru 10165 points

Part Number: 66AK2G12

Hi Support Team,

Our customer is using 66AK2G12ABY100, and is considering switching to the following temperature-extended product due to a heat issue.
I have checked the datasheet and it seems that the only difference between ABYA and ABYT is the operating temperature,
and is it correct that there is no difference in pins, specifications, etc.?
Please let me check just to be sure.

Items under consideration
(extended temperature product)
- 66AK2G12ABYA100
- 66AK2G12ABYT100

Best Regards,
Kanae

  • Kanae

    Yes no other difference apart from the temperature specification/coverage. 

    Additionally if they are planning to run at Tj beyond 105C , they should also look at the POH table in the datasheet:5.3 Power-On-Hour (POH) Limits 

    We only provide guidance for POH assuming that the use-case is 24/7 100% at 125 Tj 

    Regards

    Mukul