This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: What is the maximum camera resolution that MIPI CSI-2 can support?

Part Number: TDA4AL-Q1

Hi Expert,

What is the maximum camera resolution that MIPI CSI-2 can support? The datasheet says it is 4M? Because there are 2M*8 input at the same time, it should be 16M

If two CSI-2 are input at the same time, will the maximum resolution be affected?

Can VPAC handle 2 CSI-2 inputs at the same time?

Thanks

Daniel