This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: Change PMIC state from ACTIVE to MCU only mode

Part Number: SK-TDA4VM

Hi,

I'm trying to change PMIC state from active to mcuonly as part of mcuonly mode entry sequence, but the main domain is not getting turned off. 

I'm using "Lpm_pmicStateChangeActiveToMCUOnly()" api from lpm example for state change. After calling the api, main domain is still on. But the same api when i called in j721E EVM board, I can see LED LD5 is turned off. Is there any change in configuration for SK-board? 

How to change the PMIC state from Active to MCU only in SK-Board?

J721E EVM board having same PMIC's as SK-Board mentioned below.

SK- Board details:

J721EXSKG01EVM (PROC112A1)

PMICA - PTPS659X XXXX-Q1

PMICB - TPS659411-Q1

processor-sdk-rtos-j721e-evm-09_01_00_06