I use DM368 to encode the video.The input is 1600x1200,YUV data.
If I set the bitrate is 5M,the performance is very good even if I move the image .
if I set the bitrate is 2.5M, the performance is also good with the still image.
But if move the image ,the performance is very bad .
There are more blocks in the video streams.
I do not know why.
The dvsdk is 2.10.01.18.The h264 codes is 02.30.00.01 and the release followed by this codec is validated .
The following is the paraments.