This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A3: GPIO bank interrupts mapping

Part Number: AM62A3

Hi all,

the TRM for the AM62A is not very clear about exactly which GPIOx interrupts are mapped to which GPIOx_GPIO_BANK_y interrupts. Is there a clear mapping somewhere?

The TRM contains a Table 10-5 for MAIN_GPIOMUX_INTROUTER0_INTERRUPT_MAP, which lists all the GPIO interrupts and GPIO bank interrupts at the input of the router. But it is not clear which interrupts feed into the each bank.

...

The same is needed for the MCU_GPIO0_GPIO_BANK_y interrupts

Please let us know how this is mapped.

Thanks!

--Gunter