hi all
as i know, GPIOs on tps65930 can be accessed by "omap_request_gpio(OMAP_MAX_GPIO_LINES + *)" in linux kernel, but how can i access them in U-boot ?
thaks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
we the tps65950. You can use i2c register commands to access the gpio control registers like this:
i2c md 49 aa.1 1
(read one byte from i2c chip 0x49, register 0xaa GPIO_CTRL)
i2c mw 49 aa.1 00
(write a byte to i2c chip 0x49, register 0xaa GPIO_CTRL)
Make sure you use the physical register address, not the address offset.
thanks,
i just found the datasheet:
http://www.google.com.hk/url?sa=t&source=web&cd=1&ved=0CC0QFjAA&url=http%3A%2F%2Ffocus.ti.com%2Fgeneral%2Fdocs%2Flit%2Fgetliterature.tsp%3FliteratureNumber%3Dswcu050g%26fileType%3Dpdf&ei=SpJ5TrXTB9GuiQe7uoUa&usg=AFQjCNE89cREBjmjhhAd5L43w8Z3vDOH4Q