Other Parts Discussed in Thread: UNIFLASH
Hi Expert,
We are working on custom board based on EVM.
1. We have selected UART boot mode on our board, but we are unable to flash the binaries into OSPI flash through uniflash CLI.
2. When i run the command to flash the flash writer, it completes the flash writer into internal RAM. But after the flash writer when i run the command to flash the SBL it stuck after transfer the header of the SBL.


3. The part no of the OSPI flash (S28HS512TGABHM010) is same as EVM.
when i run the run the example of ospi_flash_app_test from SDK through JATG for validate the flash it passes all the tests.

Do you have any suggestions?
Regards,
Satyajeet Singh