Part Number: TMDS64EVM
Hello TI support team.
Please tell me about UART reception using DMA.
I'm using mcu_plus_sdk_am64x_08_06_00_45.
The referenced project is uart_echo_dma_am64x-evm_r5fss0-0_nortos_ti-arm-clang.
I am trying to periodically receive 8 bytes of data from a PC using a timer.
The PC sends 8 bytes of data to the EVM in synchronization with the CR5 timer.
I am calling UART_read inside CR5's 4kHz timer interrupt handler.
When I receive 8 bytes of data from the PC, I'm expecting a DMA transfer end interrupt, but it stops as shown below.

What does this mean?
Also, shouldn't UART_read be called inside an interrupt handler?
Best regards,
Kiyomasa Imaizumi.