This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6411: Clause 45 support

Part Number: AM6411
Other Parts Discussed in Thread: SYSCONFIG

Hello,

I try to enable Clause 45 support via sysconfig for our custom board but the software keeps failing and debug print on terminal states "Clause 45 is not supported".

According to the reference manual CPSW supports both clause 22 and clause 45, but single stepping through the code I found the following in mdio.c, line 233:

    if (mdioCfg->c45EnMask != ENET_MDIO_PHY_ADDR_MASK_NONE)
    {
        status = ENET_ENOTSUPPORTED;
        ENETTRACE_WARN("MDIO Clause 45 is not supported\n");
    }

is this a bug? or something not yet implemented in the SDK? or am I doing something wrong?

I am using mcu_plus_sdk_am64x_09_01_00_41.

Thank you for your help,

Paolo Mattachini