Other Parts Discussed in Thread: OMAP-L138
Hi All,
I recently received a OMAP-L138 kit from TI. It works nicely with the sample SD card Linux. Now I want to build a setup more suitable to my intended application.
The SD card is split into two partitions. The first is a FAT32 the second ext3, the first is offset by 21.
All the DIP switches are set to OFF as instructed by the manual. With no SD card present I get the message.
SD/MMC Boot failed.
From this I deduce that the U-Boot loader is not on the SPI-Flash, and is loaded from the SD Card.
So my questions are:
1. What is in the first 20 'blocks' of the SD Card ?
2. Is there a utility to construct an with a valid layout that will at least start u-boot ?
3. Can I place u-boot in the SPI flash ? if so waht is the safest procedure ?
If these are FAQs, I apologise but any help, including pointers to the appropriate documentation, much appreciated.
Regards,
Andrew