Our customer has MMC1 ntermoittent read error on their board
and investigating the problem.
They are using VDD1 at OPP1G.
Please answer following our questions.
DM3730 Data Manual(SPRS685D) pae 2 describes as follows.
1.8-V I/O and 3.0-V (MMC1 only),
0.9-V to 1.2-V Adaptive Processor Core Voltage
0.9-V to 1.1-V Adaptive Core Logic Voltage
Note: These are default Operating Performance
be optimized to lower values using
SmartReflex AVS.Point (OPP) voltages and could
I think MMC could use with OPP1G operationg point, but above "0.9-V to 1.2-V Processor Core Voltage"
is OPP50 and OPP100(not OPP1G).
Please confirm my understanding that MMC can oprerate with OPP1G.
Also, please explain the meaning of above description pf page 2.
Regards.