Other Parts Discussed in Thread: MSP430FR5969
I'm using an MSP430FR5969 with the compiler ti-cgt-msp430_18.12.4.LTS, and I'd like use the alternative vector table location, which is the top of the RAM. In the generated linker command file I'm seeing the following line in the sections:
.stack : {} > RAM (HIGH) /* Software system stack */
Based on that the stack is also starting from the top of the RAM. As a linker option I know how to set the size of the stack, but how change the starting address? The original RAM range is 0x1C00 - 0x2400, ideally I'd change the stack to start from 0x2388, and the vector table would be at 0x2390 - 2400.
Anyway is there any documentation which describes the linked command file in detail? I've only found this, but it doesn't dive too deeply: software-dl.ti.com/.../sdto_cgt_Linker-Command-File-Primer.html